2023-07-14 12:31 AM - edited 2023-08-01 04:27 AM
Hello,
I have referred to the tutorial documents from the University of Texas at Austin and I am using STM32CubeIDE. I generated a 1V amplitude 10kHz sine wave using a signal generator. After processing it through STM32H735G-DK, I observed a 10kHz sine wave with an amplitude of 0.6V on the oscilloscope. I am unsure of the errors in the code and unable to find a solution.
Sincerely,
kuxiang
2023-07-14 01:33 AM
Hi @kuxiang,
Welcome to ST Community!
I suggest you double check the steps you followed referring to the following knowledge articles:
For sure you can replace the NUCLEO-G070RB by your own board in the steps of the tutorial.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.