Skip to main content
Associate II
March 27, 2024
Solved

stm32h723zg Clause 45 MDIO

  • March 27, 2024
  • 7 replies
  • 1890 views

Hi all,

i see H7 supports clause 45 MDIO access, but in the HAL library looks not implemented, i see only clause 22.

How should i proceed to read/write c45 ?

 Thanks,

angelo

Best answer by mƎALLEm

Hello,

I've got a feedback regarding that request. The decision was not to add Clause45 support for the actual product including H7 for many reason including the fact that there is no ST STM32 development kits is equipped with a Clause45-capable PHY. But Clause45 (maybe) it will be addressed in the HAL of newer products.

7 replies

mƎALLEm
ST Technical Moderator
March 27, 2024

Hello,

Which MDIO interface you are talking about? is it the MDIO of the ETH or the MDIO slave (MDIOS)?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
heisenbugAuthor
Associate II
March 27, 2024

MDIO inside the ETH IP

heisenbugAuthor
Associate II
March 27, 2024

Well, found now that the PHY chip i am using is supporting C22 to C45 bridge (multiple devices addressing), so don't need to add Clause 45 to HAL. Anyway, since h7 supports Clause 45, would be nice to have it imnplemented in HAL.  

mƎALLEm
ST Technical Moderator
October 7, 2024

Hello,

Internal ticket already raised for follow-up 177202

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
February 26, 2025

Hello,

I've got a feedback regarding that request. The decision was not to add Clause45 support for the actual product including H7 for many reason including the fact that there is no ST STM32 development kits is equipped with a Clause45-capable PHY. But Clause45 (maybe) it will be addressed in the HAL of newer products.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Visitor II
October 11, 2025

STM32H7 clause 45 is supported by the chip, but not by the HAL library; Or does the chip itself not support it?

Pavel A.
October 11, 2025

@leo2025 Is your request related to the *slave* MDIO (MDIOS) of STM32F7, H7? The ETH of STM32 MCUs is not GBe anyway. If your advanced PHY has other host interfaces besides MDIO (I2C, SPI) consider using these.

Visitor II
October 11, 2025

yeah, I need the mdio interface of the STM32H7xx Mac to read DSP 32-bit register data, and I don't need to use RMII or MII

Pavel A.
October 13, 2025

 read DSP 32-bit register data

Hmm then maybe bit-bang the C45 MDIO protocol ?

heisenbugAuthor
Associate II
October 14, 2025

Hi,

at least for stm32h7xx, both Clause 22 and 45 are supported in hardware.

What does it mean: that if you set c45e bit as 0 (default) the MDIO controller sends out data as per Clause 22. If c45e is set to 1, it sends C45.

I already added the functionality into HAL one year ago. 

https://github.com/STMicroelectronics/stm32h7xx-hal-driver/pull/51/commits/00928b443eaedabae4a47aa2210b3ce5c84b4adb

After long time waiting, probably one year or so, as you can see in the PR, ST replied i didn't signed a specific CLA agreement and the PR is refused. I decided to refuse also to spend time on this. Anyway, my commit works and you can use it from my PR.

regards,
Angelo Dureghello

 

Visitor II
October 15, 2025

Thank you for your contribution!!

heisenbugAuthor
Associate II
October 17, 2025

Just to be correct, i've read an older PR. Reason for refusing this is that ST cannot test this since there are no ST dev kits with clause45 phy. I tested this from Zephyr just soldering 2 mdio wires to an Analog Devices dev board (adin1100), and opening the 2 lines in the nucleo.