cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H723 DACs

Repwoc
Associate III

The datasheet for STM32H723VG (https://www.st.com/en/microcontrollers-microprocessors/stm32h723vg.html) states that the devices have 2 x 12 bit, 2-channel DACs. 

Repwoc_1-1733832699606.png

However, in STM32CubeMX I see only one DAC listed (device = STM32H723VGT6).

Repwoc_0-1733832663426.png

Is this an error in the datasheet or an issue with STM32CubeMX?  Or something else?

 

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

STM32H7 has one DAC instance DAC1 with two output channels on DAC1_OUT1 / DAC1_OUT2.

From the reference manual:

SofLit_0-1733835274854.png

Almost the same same question asked in this thread.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

View solution in original post

5 REPLIES 5
SofLit
ST Employee

Hello,

STM32H7 has one DAC instance DAC1 with two output channels on DAC1_OUT1 / DAC1_OUT2.

From the reference manual:

SofLit_0-1733835274854.png

Almost the same same question asked in this thread.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

OK thanks.  So it appears that the datasheets are misleading at best.  I suggest that they are updated to say "1 x 12 bit, 2 channel DAC".  Then there would be no ambiguity and no confusion.

I think it's something inherited from the first F1 family and it's "misuse of language". 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.
Repwoc
Associate III

Note it's the "Product overview" web page linked to above that states 2 x 12-bit, 2-channel DACs, not the datasheet.


@Repwoc wrote:

Note it's the "Product overview" web page linked to above that states 2 x 12-bit, 2-channel DACs, not the datasheet.


I will escalate that internally to fix the web page.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.