2021-04-30 3:38 AM
Hi team,
I'm using STM32H753BI. Here i'm using USART1 (PA9 & PA10) in DMA Mode. That code is generated by cubeMX and also i tried the example program of STM32H743-EVAL Board. Both are not working.
Here i have attached the hal_msp_file.c and main.c for your reference.
Thanks,
vel.
Solved! Go to Solution.
2021-05-04 12:04 AM
Tx buffer (aTxStartMessage) is at 0x20000000 and that's DTCM which is not accessible by DMA.
JW
2021-04-30 7:56 AM
What does "not working" mean here specifically? How do you know it's not working?
2021-04-30 8:13 AM
DMA does work on the H7/UART
I suspect you're going to have to be more attentive to the memory buffer addresses, cache coherency, and program flow here.
2021-04-30 5:05 PM
Hi,
Thanks for your response. I'm expecting the data in Hyper terminal. But data was not shown the terminal. That's why i mentioned its not working.
2021-04-30 5:59 PM
If the interrupt and polled versions transmit successfully the UART works.
If the DMA isn't sending the expected data, check the buffer address
2021-05-02 11:13 PM
Hi,
Yes, interrupt and polled version transmission is working fine.
verified the buffer address, it is correct.
HAL_DMA_ERROR_TE error bit was set while transmitting the data.
2021-05-02 11:51 PM
> verified the buffer address
Tell us that address.
JW
2021-05-02 11:54 PM
Hi,
Thanks for your response. I understand your point. That's why I'm follow the example program for STM32H743I-EVAL Board example. but example program also not working.
HAL_DMA_ERROR_TE error bit was set while transmitting the data.
2021-05-03 9:29 PM
Hi,
Thanks for your response. Here I'm mentioned the DAM Address. Buffer Address is 0x400200xx..
Thanks,
vel
2021-05-04 12:04 AM
Tx buffer (aTxStartMessage) is at 0x20000000 and that's DTCM which is not accessible by DMA.
JW