Skip to main content
JShro
Associate III
December 30, 2019
Question

STM32H7 triggering a SPI TX transmission via DMA with a synch event on EXTI0

  • December 30, 2019
  • 20 replies
  • 8105 views

Hi All,

Looking at the STM32H7 Ref manual it seems the DMAMUX would allow for a DMA channel to be synchronized with an external event on the EXTI0 input.

I would like to use this capability to trigger an SPI transmission to an ADC (since this would allow me to avoid time consuming tasks in the ISR routines )

I figured I would be able to configure the SPI2 TX in DMA mode and enable the DMA request synchronization settings so I have the following configuration.

SPI2 TX is assigned to DMA1 Stream 0. and the DMA Request synchronization settings are setup for

Enable Synchronization

Synchronization signal EXTI0

SignalPolarity: Synchronize on falling edge

Request Number: 1

The SPI initialization is as follows

hdma_spi2_tx.Instance = DMA1_Stream0;
 hdma_spi2_tx.Init.Request = DMA_REQUEST_SPI2_TX;
 hdma_spi2_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
 hdma_spi2_tx.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_spi2_tx.Init.MemInc = DMA_MINC_DISABLE;
 hdma_spi2_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
 hdma_spi2_tx.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
 hdma_spi2_tx.Init.Mode = DMA_CIRCULAR; //DMA_NORMAL;
 hdma_spi2_tx.Init.Priority = DMA_PRIORITY_MEDIUM;
 hdma_spi2_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
 if (HAL_DMA_Init(&hdma_spi2_tx) != HAL_OK)
 {
 Error_Handler();
 }
 
 pSyncConfig.SyncSignalID = HAL_DMAMUX1_SYNC_EXTI0;
 pSyncConfig.SyncPolarity = HAL_DMAMUX_SYNC_FALLING;
 pSyncConfig.SyncEnable = ENABLE;
 pSyncConfig.EventEnable = DISABLE;
 pSyncConfig.RequestNumber = 1;
 if (HAL_DMAEx_ConfigMuxSync(&hdma_spi2_tx, &pSyncConfig) != HAL_OK)
 {
 Error_Handler();
 }
 
 __HAL_LINKDMA(hspi,hdmatx,hdma_spi2_tx);

The EXTI input is configured as follows

GPIO_InitStruct.Pin = SPI2_EXTI_SYNC_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
GPIO_InitStruct.Pull = GPIO_PULLDOWN; //GPIO_NOPULL;
HAL_GPIO_Init(SPI2_EXTI_SYNC_GPIO_Port, &GPIO_InitStruct);

The EXTI input is PA0 and it is driven via a PWM signal from the High resolution timer output pin connected to PA0.

I have verified that I am getting a pulse every 1 us on the EXTI input - however the SPI DMA TX is not being triggered.

Any thoughts on if this is an appropriate way to achieve the desired outcome or am I missing something?

Thanks

Jay

This topic has been closed for replies.

20 replies

waclawek.jan
Super User
December 30, 2019

You don't want to synchronize, but to generate an event. Read the DMAMUX chapter in RM, DMAMUX request generator subchapter.

JW

PS. The signals naming is a hopeless mess, extit0 in DMAMUX chapter, exti_exti0_it in the interconnections chapter, exti_exti0_wkup in NVIC chapter, probably all denoting the same signal, neither of which is mentioned in the EXTI chapter... @Vincent Onde​ 

JShro
JShroAuthor
Associate III
December 30, 2019

Hi Jan,

Thanks for the input - but I think I am even more confused now... Please bear with me for a moment as I try to clarify...

I read the DMAMUX chapter but it is a bit confusing for me so just to clarify my understanding here's is how I interpreted it - please correct my misunderstanding...

The block diagram - copied below

0690X00000BvV5FQAV.png

Seems to indicate that we can have a DMA_REQUEST from peripheral not processed until a Synchronization input is present.

In my case I was hoping to achieve the following...

I was assigning the DMA1_STREAM0 channel to SPI2_TX. (I request a DMA TX operation by invoking the following in the code)

 /* Enable the Tx DMA Stream/Channel */
 if (HAL_OK != HAL_DMA_Start_IT(hspi2.hdmatx, (uint32_t)aTxBufferNormal, (uint32_t)&(hspi2.Instance->TXDR), 1))
 {
 /* Update SPI error code */
 SET_BIT(hspi2.ErrorCode, HAL_SPI_ERROR_DMA);
 errorcode = HAL_ERROR;
 hspi2.State = HAL_SPI_STATE_READY;
 return errorcode;
 }
 
 
 // MODIFY_REG(hspi2.Instance->CR2, SPI_CR2_TSIZE, 1);
 
 
 /* Enable Tx DMA Request */
 SET_BIT(hspi2.Instance->CFG1, SPI_CFG1_TXDMAEN);
 
 /* Enable the SPI Error Interrupt Bit */
 __HAL_SPI_ENABLE_IT(&hspi2, (SPI_IT_OVR | SPI_IT_UDR | SPI_IT_FRE | SPI_IT_MODF));
 
 /* Enable SPI peripheral */
 __HAL_SPI_ENABLE(&hspi2);
 
 
 /* Master transfer start */
 SET_BIT(hspi2.Instance->CR1, SPI_CR1_CSTART);

The intent was that until the exti input (on PA0 ) goes from high to low - falling edge trigger - the DMA transaction that was setup would not be executed since the synch input condition has not been met.

I was assuming that by setting up the DMAMUX in the following fashion

pSyncConfig.SyncSignalID = HAL_DMAMUX1_SYNC_EXTI0;
 pSyncConfig.SyncPolarity = HAL_DMAMUX_SYNC_FALLING;
 pSyncConfig.SyncEnable = ENABLE;
 pSyncConfig.EventEnable = DISABLE;
 pSyncConfig.RequestNumber = 1;
 if (HAL_DMAEx_ConfigMuxSync(&hdma_spi2_tx, &pSyncConfig) != HAL_OK)
 {
 Error_Handler();
 }

I was basically telling the DMA subsystem to not start the SPI2_TX DMA transaction until the exti input goes from high to low.. - is that not the case?

What is interesting is that with the above setup if I manually toggle bit PR1 in register CPUPR1 the transmission happens (in fact I can toggle any bit but PR0) in the CPUPR1 register and the SPI transmission is initiated... - Obviously the intent was to have the PR0 flag automatically trigger the TX but that does not occur...

I think what you are suggesting is setting up the DMAMUX request generator and using the EXTI input as a trigger to write to the SPI TXDR register directly? - That could work but I am a bit confused as to why the above setup should not work especially since the block diagram seems to indicate that this scheme is feasible - but again as I mentioned initially I am still confused on exactly how the DMAMUX works and the empirical results I am getting are confusing me even more...

Really appreciate any help in clearing up my confusion.

Thanks!

Jay

waclawek.jan
Super User
December 31, 2019

I misunderstood your - you indeed appear to need the synchronization feature of DMAMUX.

I don't use the 'H7 nor DMAMUX, but I doubt there are many users here who do (other than using the straightforward request mapping).

I also don't use Cube. I believe in this case you should also stop talking in terms of Cube/HAL and start discussing directly registers content.

> What is interesting is that with the above setup if I manually toggle bit PR1 in register CPUPR1

How? You can only clear bits in CPUPR1, its bits are rc1.

But, as you write the register (and register bits can't be written alone, hardware always writes at least a byte) there may be some mechanism in hardware which generates an edge on the output signal which then goes into DMAMUX. This is not well described in the manual (as I wrote above, it's not clear at all what the signal which goes into DMAMUX really is).

But talking about EXTI_CPUPR1, you should be able to *see* that the selected edge occured, that should set this register's bit 0. You should be also able to set it indirectly by setting the respective bit in EXTI_SWIER1.

As an experiment, you can also enable the respective EXTI0 interrupt and write a simple ISR for it to check it is working - e.g. toggle a pin observed by LA.

That in turn should generate the required edge in the synchronization input of DMAMUX. Check the respective DMAMUX1_CxCR register, if the proper SYNC_ID and proper DMAREQ_ID (i.e. the number corresponding to SPI2_TX) is set in it.

JW

JShro
JShroAuthor
Associate III
December 31, 2019

>How? You can only clear bits in CPUPR1, its bits are rc1.

I was just toggling it in the system view window under uvision but that made me think some more about what you said below ...

>As an experiment, you can also enable the respective EXTI0 interrupt and write a simple ISR for it to check it is working - e.g. toggle a pin observed by LA.

Yes I did that and lo and behold the SPI started working. :o . It seems the internal routing must require the int to be serviced for the DMAMUX to be notified - makes no sense to me still... Since this means I am wasting time in the ISR (even if it is simply to service the ISR) basically I was hoping to start the SPI transmission immediately after the EXTI_IT edge detection but as it stands the ISR takes up 230 ns so the SPI transmission is delayed by that much time which will not allow me to meet the timing spec for the A/D converter that I am talking to

So maybe I need to look for a better synch signal - however I am assuming any synch input will behave in the same way - can any one from ST confirm?

Thanks

Jay

waclawek.jan
Super User
December 31, 2019

Interesting.

Can you please try the other (rising edge) polarity set for the synchronization input in DMAMUX?

JW

JShro
JShroAuthor
Associate III
January 1, 2020

Just checked that also - it seems the polarity does not matter both rising & falling edge require the ISR to be enabled - would love to understand the reason behind this as it seems very inefficient to have to do it this way. Hope someone from ST can shed some light

Thanks

berendi
Principal
January 1, 2020

If it doesn't work out with EXTI, then see if you can route the external signal to a timer channel.

Then you can set up the timer channel in capture mode, and issue a DMA request on capture to write the SPI TX register.

waclawek.jan
Super User
January 1, 2020

> both rising & falling edge require the ISR to be enabled -

I did not expect this to go away - as the DMAMUX synchro is edge-driven, there must be something which clears the pending exti0-interrupt signal, so that the next edge could be generated. I expected to see the interrupt-caused latency to go away with the opposite polarity.

To avoid the interrupt yet still clear the pending interrupt, you could perhaps use another DMAMUX channel to generate a DMA from the same exti0-interrupt, which would write the appropriate constant into EXTI_CPUPR1 clearing the pending interrupt.

Or, use the workaround outlined by berendi above.

JW

NPato
Associate III
February 4, 2020

Hi,

I had a very similar problem and ended up routing the external signal in via LPTIM1 (rather than EXTI0) and using that as the synchronisation event for the DMA.

Interestingly EXTi0 can be used in DMAMUX2/BDMA directly as I've also tried this when using SPI6.

Cheers

Nigel

JShro
JShroAuthor
Associate III
February 4, 2020

Thanks for the confirmation - Yeah I ended up using LPTIM also. Still curious on why EXTI0 does not work in this scenario but I guess we will never know :sad_but_relieved_face:

waclawek.jan
Super User
February 5, 2020

> Still curious on why EXTI0 does not work in this scenario

Because, the input to DMAMUX is coming from the output of EXTI module, i.e. EXTI pending register.

>> I did not expect this to go away - as the DMAMUX synchro is edge-driven, there must be something which clears the pending exti0-interrupt signal, so that the next edge could be generated.

> Interestingly EXTi0 can be used in DMAMUX2/BDMA directly

That's because input to DMAMUX2 is not coming from EXTI module, ie. it's not the output of EXTI having been already latched, but directly from SYSCFG, i.e. it's the output of the EXTI input multiplexer, i.e. it's directly the pin assigned to given EXTI.

So the real question is, why did ST decide to wire it up in this particular manner, and also why don't they document it properly (as the bare minimum, the signal names in the DMAMUX chapter ought to match signal names in other relevant chapters).

JW

DMast.1
Associate III
November 18, 2020

Hi all, I have the same problem to interface my stm32h745 with an external 16bit ADC that start samplig with a CNV signal and tell to MCU that conversion ended sending BUSY signal down. So I interesting to understand if JShro was able to synchronize SPI communication with and external interrupt EXTI and get a interrupt on DMA read end event.

Thanks in advance

DM

JShro
JShroAuthor
Associate III
November 18, 2020

See the responses from @Community member​  That explains why EXTI will not work - I ended up using LPTIM input.

DMast.1
Associate III
November 19, 2020

So, let me explain if I understand correctly how you read out the conversion from ADC. You setup an LPTIM peripheral to generate the external CNV signal to start conversion (suppose 1MHz freq and 50% duty) and use the negative edge of this signal to synchronize the SPI DMA to get conversion from ADC setting at least 60MHz of SPI_SCK to respect the minimal timings? If this is, I suppose you use the SPI complete ISR to save data somewhere RAM memory and check the complete acquisition sequence (ex. 1000 samples)?

Thanks in advance

DM