cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 SPI2 unrealibe transmission of data

CLeo.1
Senior II

Hi everyone,

A new issue has occur and have no idea as to why the transmission would be sometimes corrupt. I try sending the word "Hello World" as a test, however sometimes I would receieve the word but sometimes I would receivbe garage values that various in size.

The setup:

void initSPI() {
 
	LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOB);
	LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOA);
	LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_SPI2);
	//LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SPI1);
 
	LL_GPIO_InitTypeDef LL_GPIO;
	LL_SPI_InitTypeDef LL_SPI;
 
	LL_GPIO_StructInit(&LL_GPIO);
	LL_SPI_StructInit(&LL_SPI);
 
	// Setting up SPI 1 GPIO
	LL_GPIO.Alternate = LL_GPIO_AF_5;
	LL_GPIO.Mode = LL_GPIO_MODE_ALTERNATE;
	LL_GPIO.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
	LL_GPIO.Pin = LL_GPIO_PIN_13 | LL_GPIO_PIN_14 | LL_GPIO_PIN_15;
	LL_GPIO.Pull = LL_GPIO_PULL_DOWN;
	LL_GPIO.Speed = LL_GPIO_SPEED_HIGH;
	LL_GPIO_Init(GPIOB, &LL_GPIO);
	LL_GPIO_StructInit(&LL_GPIO);
 
	// Setting up SPI 1 GPIO
	LL_GPIO.Alternate = 0x00;
	LL_GPIO.Mode = LL_GPIO_MODE_OUTPUT;
	LL_GPIO.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
	LL_GPIO.Pin = LL_GPIO_PIN_4;
	LL_GPIO.Pull = LL_GPIO_PULL_DOWN;
	LL_GPIO.Speed = LL_GPIO_SPEED_HIGH;
	LL_GPIO_Init(GPIOA, &LL_GPIO);
 
	// Setting up SP1 1 Peri
	LL_SPI.BaudRate = LL_SPI_BAUDRATEPRESCALER_DIV256;
	LL_SPI.BitOrder = LL_SPI_MSB_FIRST;
	LL_SPI.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE;
	LL_SPI.CRCPoly = 0x00;
	LL_SPI.ClockPhase = LL_SPI_PHASE_1EDGE;
	LL_SPI.ClockPolarity = LL_SPI_POLARITY_LOW;
	LL_SPI.DataWidth = LL_SPI_DATAWIDTH_8BIT;
	LL_SPI.Mode = LL_SPI_MODE_MASTER;
	LL_SPI.NSS = LL_SPI_NSS_SOFT;
	LL_SPI.TransferDirection = LL_SPI_FULL_DUPLEX;
	LL_SPI_Init(SPI2, &LL_SPI);
	//LL_SPI_EnableGPIOControl(SPI2);
}

The usuage:

int main(void)
{
	char* word = "Hello World";
 
	HAL_Init();
	SystemClock_Config();
 
	initSPI();
	LL_SPI_SetTransferSize(SPI2, 11);
	GPIOA->BSRR |= (1 << 4);
 
	LL_SPI_Enable(SPI2);
	LL_SPI_StartMasterTransfer(SPI2);
	GPIOA->BSRR |= (1 << 20);
 
for (int i = 0; i < 11; i++) {
	while(LL_SPI_IsActiveFlag_TXP(SPI2) == 0){};
	LL_SPI_TransmitData8(SPI2, word[i]);
}
	while(LL_SPI_IsActiveFlag_TXP(SPI2) == 0){};
	while(LL_SPI_IsActiveFlag_EOT(SPI2) == 0){};
	LL_SPI_Disable(SPI2);
	GPIOA->BSRR |= (1 << 4);
 
  while (1)
  {
 
  }
}

The problem:

0693W00000Y9GFGQA3.png0693W00000Y9GFaQAN.png0693W00000Y9GFfQAN.png0693W00000Y9GFkQAN.png

0 REPLIES 0