2018-04-06 7:43 AM
Hai, Iam using the STM32H743VIT controller , We are using the spi4 in our board ,we generated the code using the cube mx nothing is coming(CLK and SIN)when transmit the data using the function ( HAL_SPI_Transmit(SPI_HandleTypeDef *hspi, uint8_t *pData, uint16_t Size, uint32_t Timeout)). we configured the SPI to the 8 bit mode.But with the same configuration the SPI2 is working fine.
Thank you
Best regards
Maheshwar.
#uphill-skiing #stm32h7-spi-sync #stm32h7 #spi Note: this post was migrated and contained many threaded conversations, some content may be missing.Solved! Go to Solution.
2018-04-06 3:58 PM
Upgrading CubeMX is not enough.
You have to update HAL firmware to 1.2.0
In this version there are no SPI issues known.
2018-04-06 8:21 AM
Hello
maheshwarreddy681
,Which CubeMx and Firmware package version are you using? This will help us to check your issue.
Best Regards,
Imen
2018-04-06 8:51 AM
Can we use ONE thread? Probability suggests these events/observations are related.
https://community.st.com/0D50X00009XkWXISA3
2018-04-06 10:29 AM
Thank you for the valuable reply .
We are using the version 4.22.1
2018-04-06 10:38 AM
Hi
maheshwarreddy681
,You are welcome.
I recommend you to update and use latest version of STM32CubeMx version 4.25 and
v 1.2.0.Then let us know if that problem is still being faced.
Best Regards,
Imen
2018-04-06 12:55 PM
Thank you for the valuable reply .
We had updated the cube mx to the 4.25 then also same proble.
2018-04-06 3:58 PM
Upgrading CubeMX is not enough.
You have to update HAL firmware to 1.2.0
In this version there are no SPI issues known.
2018-04-06 4:05 PM
Can you please tell me . How to update the firmware. Now we are in need
On Sat 7 Apr, 2018, 2:28 AM Joerg Wagner, <st-microelectronics@jiveon.com>
2018-04-06 4:21 PM
Are you using the H7 v1.2.0, or not? The CubeMX library updater should be able to pull directly, and there is the Cube H7 download page.
http://www.st.com/en/embedded-software/stm32cubeh7.html
#uphill%20skiing
2018-04-06 4:24 PM
Yaaaa we are using same stm32h7 v2.1.0.
On Sat 7 Apr, 2018, 2:52 AM Clive One, <st-microelectronics@jiveon.com>