2016-10-20 2:10 AM
While I see no announcement, the following is online:
http://www.st.com/content/st_com/en/products/microcontrollers/stm32-32-bit-arm-cortex-mcus/stm32h7-series.html?querycriteria=productId=SS1951 Not only the 400MHz Fclk is worth mentioning, but also 1MB of RAM (64kB ITCM + 128kB DTCM, the rest is a 3-part user SRAM and 4kB backup SRAM) JW2016-10-20 6:32 AM
http://www.st.com/content/st_com/en/about/media-center/press-item.html/p3878.html
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-10-21 12:18 PM
It looks like a nice fit below an A series based controller. An M7 is a lot easier to use compared to going the A5, A7, A9 or an old ARM11 route. Forcing that jump to SDRAM from flash and internal SRAM adds a lot to the BOM cost, plus the layout hassles going to BGA and extra PCB layers.
By coincidence just after reading about the H7 I was handed a problem that needs a custom built gateway from proprietary radio to Ethernet. The H7 is fast enough to handle the thruput and large enough memory that I don't have to look at an A7. Timing for the announcement could not be better....
Jack Peacock
2016-11-16 4:43 AM
In action, http://blog.st.com/see-new-stm32h7-mcu-action/
The real stuff is from 2:15. This of course does not demonstrate the powers of 'H7xx, but that of the built-in hardware JPEG decoder. Pretty, though. A few pictures of the evalboard used in that demo: http://time4ee.com/articles.php?article_id=35 JW2016-11-16 5:14 AM
> It looks like a nice fit below an A series based controller. An M7 is a lot easier to use compared to going the A5, A7, A9 or an old ARM11 route. Forcing that jump to SDRAM from flash and internal SRAM adds a lot to the BOM cost, plus the layout hassles going to BGA and extra PCB layers.
Depends on one's viewpoint (i.e. requirements). A Cortex A (or another ''real'' CPU) allows a proper OS environment like Linux, with a huge quantity of available and free software, including developers. For certain projects, hardware design costs are less of a driving factor. With this in mind, I'm not really surprised by the rather reluctant market acceptance of M7 devices.
2016-11-16 5:22 AM
> reluctant market acceptance of M7 devices
Do you have numbers or any other fact in supporting this? Thanks, JW2016-11-16 6:37 AM
> Do you have numbers or any other fact in supporting this?
No - just statements of MCU vendor staff at trade shows. And, of course, project discussions at my company/companies that I witnessed.2016-11-16 6:45 AM
To add another comment:
Does not speak the number of available M7 silicons (and the number of M7 licensees) speak for itself ? But that might as well have to do with the ongoing ''consolidation process'' in the MCU world (which gives me kind of a headache ...).2016-11-23 4:05 AM
Here
about a multi-vendor round table discussion, coming to similar conclusions. However, in German language.2016-11-23 4:55 AM
Thanks, AvaTar.
Jan