STM32H7 Option bytes programming halts CPU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-31 12:44 AM
The MCU halts for approximately 300ms after setting the OPTSTART bit in the FLASH_OPTCR register. In HAL_FLASH_OB_Launch() :
HAL_StatusTypeDef HAL_FLASH_OB_Launch(void)
{
HAL_StatusTypeDef status;
/* Wait for CRC computation to be completed */
if (FLASH_CRC_WaitForLastOperation((uint32_t)FLASH_TIMEOUT_VALUE, FLASH_BANK_1) != HAL_OK)
{
status = HAL_ERROR;
}
#if defined (DUAL_BANK)
else if (FLASH_CRC_WaitForLastOperation((uint32_t)FLASH_TIMEOUT_VALUE, FLASH_BANK_2) != HAL_OK)
{
status = HAL_ERROR;
}
#endif /* DUAL_BANK */
else
{
status = HAL_OK;
}
if (status == HAL_OK)
{
/* Set OPTSTRT Bit */
SET_BIT(FLASH->OPTCR, FLASH_OPTCR_OPTSTART);
/* Wait for OB change operation to be completed */
status = FLASH_OB_WaitForLastOperation((uint32_t)FLASH_TIMEOUT_VALUE);
}
return status;
}
I tested this on the STM32H743I-EVAL2 eval board and I didn't find any information in the ST documentation.
When OPTSTART bit is set, the embedded Flash memory launches the option byte modification in its non-volatile memory and updates the option byte registers with _CUR extension.
That can explain a little delay but 300ms seems way too long.
Thanks for your help
Solved! Go to Solution.
- Labels:
-
Flash
-
STM32H7 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-01 9:49 AM
Hello @NilocA​,
The CPU is stalled during the write to Flash (erase/programming)
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-31 3:50 AM
Datasheet says 1 to 4 seconds sector erase time for 128kByte sector. The option bytes sector is certainly much smaller, but erase time in the order of several 100ms seems plausible.
​
Note that the option bytes flash cells are not EEPROM cells, i.e. the whole block is erased, then reprogrammed. This even suggests that option byte programming is a rather delicate operation. Any power glitch in the meantime and ...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-01 9:49 AM
Hello @NilocA​,
The CPU is stalled during the write to Flash (erase/programming)
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.