cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H5 GPDMA Timer circular buffering interrupt issue

alessioschisano
Associate

Hi, 

I am using linked list mode for circular buffering DMA with Timer1 in burst mode. The expectation is that after 300 transfer from memory to timer 1 CCR register, the DMA should start again with the buffer. To do that I need to use Half Trasfer interrupt and Transfer complete interrupt to elaborate the buffer. 

 

It happen something strange, I receive interrupt for each data transferred from memory to peripheral, instead of the half/complete transfer, so I cannot process the buffer. 

Here is my configuration:

 

 

//Setting of DMA Burst for Timer dmacfg.Request = req; dmacfg.DestAddress = dest; dmacfg.Direction = LL_DMA_DIRECTION_MEMORY_TO_PERIPH; dmacfg.BlkHWRequest = LL_DMA_HWREQUEST_BLK;//LL_DMA_HWREQUEST_SINGLEBURST; dmacfg.DataAlignment = LL_DMA_DATA_ALIGN_ZEROPADD; dmacfg.SrcBurstLength = srclen; dmacfg.DestBurstLength = dstlen; dmacfg.SrcDataWidth = LL_DMA_SRC_DATAWIDTH_HALFWORD; dmacfg.DestDataWidth = LL_DMA_DEST_DATAWIDTH_HALFWORD; dmacfg.SrcIncMode = LL_DMA_SRC_INCREMENT; dmacfg.DestIncMode = LL_DMA_DEST_FIXED; dmacfg.Priority = LL_DMA_HIGH_PRIORITY; dmacfg.SrcAllocatedPort = LL_DMA_SRC_ALLOCATED_PORT0; dmacfg.DestAllocatedPort = LL_DMA_DEST_ALLOCATED_PORT1; dmacfg.Mode = LL_DMA_NORMAL;//LL_DMA_PFCTRL;

 

I am using Channel 0 and 1 of GPDMA2. I did some test and I can get it working with Channel 0 and 7. 

The linked list is made of only one item for updating the source address. 

 

Have someone already experienced this kind of issue?

 

Thank you

1 REPLY 1
Imen.D
ST Employee

Hello @alessioschisano ,

Did you check the related DMA units/channels and trigger sources.

I advise you to refer to this STM32H5 MOOC: - GPDMA - Basic configurationThe purpose of this part is demonstration of GPDMA simple configuration on NUCLEO-H563ZI board.

You can also refer to this article on how to configure the GPDMA using STM32CubeIDE: 

How to configure the GPDMA - STMicroelectronics Community and to this AN5593: How to use the GPDMA for STM32 MCUs application note.

Hope this helps you!

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen