cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G474VET3: pin names for motor controller PWM out question

sag
Associate III

HI I need to know the pin names for motor controller PWM out 

PWM High and PWM LOW

i can not directly PWM out function for pins

Also need capture control pin details to measure the PWM.

As i have to assign these pins for controller

1 ACCEPTED SOLUTION

Accepted Solutions

eg, for the High Resolution Timer (HRTIM):

AndrewNeil_0-1713950383553.png

 

have you also looked at Application Note AN4013, Introduction to timers for STM32 MCUs:

https://www.st.com/resource/en/application_note/an4013-introduction-to-timers-for-stm32-mcus-stmicroelectronics.pdf

 

View solution in original post

7 REPLIES 7

All the pin names & Alternate Functions are listed in the chip's datasheet.

TIM17_BKIN,
USB_CRS_SYNC,
I2C2_SMBA,
SPI2_MISO,
TIM1_CH3,
USART1_RX,
COMP6_OUT,
TIM2_CH4,
TIM8_BKIN, SAI1_D1,
SAI1_SD_A,
EVENTOUT

 

 

Where is the PWMout from above alternate fucntions?

or how can check CCP for pwm measurement

You'll also need to look in the Timer descriptions in the Reference Manual - that'll tell you what Alternate Functions are used ...

Are you aware of it? 

Reference manual is fine, but still i didnt found straight away? like other controllers alternate fucntions showos EPWM or PWM

eg, for the High Resolution Timer (HRTIM):

AndrewNeil_0-1713950383553.png

 

have you also looked at Application Note AN4013, Introduction to timers for STM32 MCUs:

https://www.st.com/resource/en/application_note/an4013-introduction-to-timers-for-stm32-mcus-stmicroelectronics.pdf

 

Thanks Andrew for your quick support.

Yes this will work fine for for pwm.

Also input capture compare for any pwm incoming signal will use below TIMx_CCRx

 

sag_0-1713951135437.png

 

sag
Associate III

Hope i can see CCR pins in datasheet for input pwm capture