2024-04-25 03:19 AM - last edited on 2024-04-25 05:49 PM by SofLit
As i am using inside comparators.
For that i can see below available options for reference voltages.
My question is about DAC output can it be set internally or i have to make physical connection by DAC out put pin to comparator input
Solved! Go to Solution.
2024-04-25 03:51 AM
2024-04-25 03:24 AM - edited 2024-04-25 03:29 AM
see in rm:
So internal DAC connection possible.
Just try in CubeMX , it shows , what you can select as internal connection.
example:
2024-04-25 03:51 AM
Yes will check
As i am in the need of variable Vre