2023-09-04 05:02 AM
Hi everyone,
I have a hardware problem with STM32G474RE on startup. If I try to supply this MCU directly from the lab power supply, it runs correctly, but when I have dips or drops or fast switching on the supply, I notice that the MCU doesn't start. I measured time when it's ok and it looked like 100ms - for me it's too long. Of course, I supply it according to specification and now I don't have any idea what is the problem.
PS. Now I connect only MCU, proper supply, RST pullup, external XTAL and one LED to notify that MCU works ok and I still have the same issue.
2023-09-05 01:40 PM
Hello @DKlew.1,
There are a few factors you can take in consideration, please look at the following aspects in more detail:
How to make sure the STM32 starts properly in our design?
Hope this helped you!
Imen
2023-09-06 09:01 AM
> I measured time when it's ok and it looked like 100ms - for me it's too long.
What time? What code are you executing? Any Cube/HAL? Try to get rid of. Try not to use Xtal (HSE/LSE?), maybe that's the source of problems. If the 'G4 has BOD, use it.
Tomas Dresler's FAQ appears to be very comprehensive, well worth posting link to it twice!
JW