2024-11-08 3:10 PM
Hi there,
I am configuring HRTIM TIMD to generate PWM which works as expected, roughly following the Synchronous Buck Converter example for the DPOW1 eval board (my target is the nucleo64).
I use LL API calls instead of HAL calls for my project. I have configured an interrup handler to service the JEOC interrupt before calling LL_ADC_INJ_ReadConversionData12() (? - not even sure if this is correct). I do not see my interrupt handler being called so either:
a) ADC conversion is not being triggered, or,
b) ADC conversion is triggered but interrupt JEOC isn't being generated.
Can someone suggest a way of ruling out one or the other problem? For example, is there a blocking LL API call that will allow reading of completed conversions? Is there an example of this somewhere for reference?
Thanks for any help in advance.
Solved! Go to Solution.
2024-11-08 9:07 PM
Fixed. I was missing calls to enable the interrupt:
NVIC_SetPriority(ADC1_2_IRQn, 0);
NVIC_EnableIRQ(ADC1_2_IRQn);
2024-11-08 9:07 PM
Fixed. I was missing calls to enable the interrupt:
NVIC_SetPriority(ADC1_2_IRQn, 0);
NVIC_EnableIRQ(ADC1_2_IRQn);