2024-02-06 8:01 AM
Hello,
I tried to execute the demo for the STM32G474E EVAL1 explained in this document : STM32CubeG4 STM32G474E-EVAL demonstration firmware - User manual.
But, I have an error when the board tries to display the pictures which are on the SD card.
I got " Error popup resource file missing please update sd card content".
I checked the SD card and my files are well in the right directory.
I tried with two different SD cards and I have the same issue.
When I checked with the debugger, I have the impression that is a problem during the initialization of the SD card during the call of SD_GoIdleState()
But now I have no idea to go further in my investigation.
So I search some help to solve my issue
Solved! Go to Solution.
2024-02-15 1:03 AM - edited 2024-02-15 1:41 AM
Not easy to recover a broken SDcard slot. May be you need to clean it but it's risky.
Or buy add an external SDcard slot module like this one and wire it yourself:
PS: take care of the pull up resistors mounted on the module (see the image).
2024-02-06 9:06 AM
Hello,
@twinest wrote:
Hello,
I tried to execute the demo for the STM32G474E EVAL1 explained in this document : STM32CubeG4 STM32G474E-EVAL demonstration firmware - User manual.
But, I have an error when the board tries to display the pictures which are on the SD card.
Which example you are running?
Which files you have stored on the SDcard?
2024-02-07 12:05 AM
Hello,
I run the example "Demo" when I choose my MCU in STM32CubeIDE in the tab "Example Selector" when I create a new project.
And I use the SD card provided with the evaluation kit and I checked, the files needed for this demo are well in the SD card.
The file system of the SD card is :
STFILES (with the bmp images used by the demo)
USER
STM32.TXT
2024-02-13 11:58 PM
Hello,
Do you have some news about my issue ?
Best regards
2024-02-14 12:15 AM - edited 2024-02-14 12:15 AM
Did you try the example provided in STM32CubeG4 under the path \Projects\NUCLEO-G474RE\Applications\FatFs as it is?
2024-02-14 12:32 AM
No, I tried only example provide for the STM32G474E EVAL1 because I have this card.
I will try this example
2024-02-14 12:54 AM
Sorry I meant under the path STM32G474E-EVAL\Applications\FatFs\FatFs_uSD_Standalone
2024-02-14 12:55 AM
No problem.
So, yes I tried this example too and I got the same error
2024-02-14 8:07 AM - edited 2024-02-14 8:10 AM
Hello,
For the demo located under Projects\STM32G474E-EVAL\Demonstrations did you copy the resources located under Projects\STM32G474E-EVAL\Demonstrations\Binary\SD_card to the SDcard?
Also are you sure the SDcard is well inserted on its slot?
2024-02-14 11:59 PM
Hello,
Yes, as I said earlier, the resources are well loaded on the SD Card, which is the SD Card provided with the board.
And the SD card is well inserted because I don't have the error related.
Like I said in my first message, I think the error occurs during the initialization of the SD card during the call of SD_GoIdleState()