cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G473 I2C2 pinout mistake in Datasheet

thomas23
Associate II

Hi,

I would like to make a new electronic design with the STM32G473, using I2C2.

But it seems there is a mistake in the datasheet regarding the pinout.

On pin description it says:

PA8 = I2C2 SDA

PA9 = I2C2 CLK

PA10 = I2C2 SMBA

Whereas on Alternate function it says:

PA8 = I2C2 SMBA

PA9 = I2C2 CLK

PA10 = I2C2 SDA

Which one is correct?

If I look on other similar MCUs, I think the second version (Alternate function) is correct, but if I check on CubeMX, it says the same as on pin description.

Thanks for your help!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Imen GH
ST Employee

​ Hello @thomas23​ ,

The pin description is the correct one:

PA8 = I2C2 SDA

PA10 = I2C2 SMBA

I will report the error to our team for correction.

Thanks for your contribution

Imen

View solution in original post

6 REPLIES 6
Imen GH
ST Employee

​Hello @thomas23​,

I will check and get back to you

Imen

Ok thanks!

Imen GH
ST Employee

​ Hello @thomas23​ ,

The pin description is the correct one:

PA8 = I2C2 SDA

PA10 = I2C2 SMBA

I will report the error to our team for correction.

Thanks for your contribution

Imen

margce
Associate III

This is still an issue even on the latest DS12712 rev4 datasheet available to download. Please be aware!

DOCon.1
Senior

Just got bitten by this; request User Manual update please.

KDJEM.1
ST Employee

Hello,

This issue is fixed and the new Datasheet revision is published in the ST website: DS12712 Rev 5.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.