2026-03-30 3:38 PM - last edited on 2026-04-14 8:47 AM by mƎALLEm
Hi,
I need to use a 5V external clock for an stm32g473. The datasheet in table 39. High-speed external user clock characteristics says Vhsel is max Vdd, but Table 12. STM32G473xB/xC/xE pin definition says PF0 / OSC_IN is FT_a (five volt tolerant).
Is it safe to use an external 5V clock ?
Thx,
Solved! Go to Solution.
2026-04-14 8:44 AM
Hello,
The design confirms that these pins are five volt tolerant only if they are used as GPIOs but the IO levels follow the levels indicated in table 39 when it is used as oscillator input i.e. they are not five volt tolerant in this case.
This applies to HSE (OSC_IN) and LSE (OSC32_IN) as well.
Hope it does answer your question.
2026-03-31 6:27 AM - edited 2026-03-31 8:16 AM
Hello,
I'm checking internally. I'll get back to you.
Internal tickets for follow-up: CDM0061203
2026-04-14 8:44 AM
Hello,
The design confirms that these pins are five volt tolerant only if they are used as GPIOs but the IO levels follow the levels indicated in table 39 when it is used as oscillator input i.e. they are not five volt tolerant in this case.
This applies to HSE (OSC_IN) and LSE (OSC32_IN) as well.
Hope it does answer your question.