2022-09-14 8:04 AM
Hello everyone,
I am trying to create a CAN project with STM32G431C8 . But there is no data in CANTX pin.
I created init codes with CubeMX and codes are below.
Here is main function;
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_FDCAN1_Init();
// MX_I2C2_Init();
// MX_SPI1_Init();
// MX_TIM4_Init();
// MX_TIM7_Init();
// MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
// main_canopen();
FDCAN_Config();
// GPIO_InitTypeDef GPIO_InitStruct = {0};
// GPIO_InitStruct.Pin = GPIO_PIN_11|GPIO_PIN_12;
// GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
// GPIO_InitStruct.Pull = GPIO_NOPULL;
// GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
// HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* USER CODE END 2 */
//HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, TxData);
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_GPIO_TogglePin(LED_RED_GPIO_Port, LED_RED_Pin);
HAL_GPIO_TogglePin(LED_GREEN_GPIO_Port, LED_GREEN_Pin);
// HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_11 | GPIO_PIN_12);
/* Set the data to be transmitted */
TxData[0] = 0x55;//ubKeyNumber1;
TxData[1] = 0x56;
TxData[2] = 0x57;
TxData[3] = 0x58;
TxData[4] = 0x59;
TxData[5] = 0x5A;
TxData[6] = 0x5A;
++TxData[7];
/* Start the Transmission process */
if (HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, TxData) != HAL_OK)
{
++ubKeyNumber1;
// if (ubKeyNumber1 == 0x4)
// {
// ubKeyNumber1 = 0x00;
// }
/* Transmission request Error */
// Error_Handler();
}
else
{
++ubKeyNumber2;
}
HAL_Delay(delay);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}fdcan.c file content;
FDCAN_HandleTypeDef hfdcan1;
/* FDCAN1 init function */
void MX_FDCAN1_Init(void)
{
/* USER CODE BEGIN FDCAN1_Init 0 */
/* USER CODE END FDCAN1_Init 0 */
/* USER CODE BEGIN FDCAN1_Init 1 */
/* USER CODE END FDCAN1_Init 1 */
hfdcan1.Instance = FDCAN1;
hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1;
hfdcan1.Init.FrameFormat = FDCAN_FRAME_FD_BRS;
hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan1.Init.AutoRetransmission = ENABLE;
hfdcan1.Init.TransmitPause = DISABLE;
hfdcan1.Init.ProtocolException = DISABLE;
hfdcan1.Init.NominalPrescaler = 1;
hfdcan1.Init.NominalSyncJumpWidth = 4;
hfdcan1.Init.NominalTimeSeg1 = 63;
hfdcan1.Init.NominalTimeSeg2 = 16;
hfdcan1.Init.DataPrescaler = 1;
hfdcan1.Init.DataSyncJumpWidth = 1;
hfdcan1.Init.DataTimeSeg1 = 5;
hfdcan1.Init.DataTimeSeg2 = 4;
hfdcan1.Init.StdFiltersNbr = 1;
hfdcan1.Init.ExtFiltersNbr = 0;
hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN FDCAN1_Init 2 */
/* USER CODE END FDCAN1_Init 2 */
}
void HAL_FDCAN_MspInit(FDCAN_HandleTypeDef* fdcanHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
if(fdcanHandle->Instance==FDCAN1)
{
/* USER CODE BEGIN FDCAN1_MspInit 0 */
/* USER CODE END FDCAN1_MspInit 0 */
/** Initializes the peripherals clocks
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_FDCAN;
PeriphClkInit.FdcanClockSelection = RCC_FDCANCLKSOURCE_PCLK1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/* FDCAN1 clock enable */
__HAL_RCC_FDCAN_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/**FDCAN1 GPIO Configuration
PA11 ------> FDCAN1_RX
PA12 ------> FDCAN1_TX
*/
GPIO_InitStruct.Pin = GPIO_PIN_11|GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF9_FDCAN1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* FDCAN1 interrupt Init */
HAL_NVIC_SetPriority(FDCAN1_IT0_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(FDCAN1_IT0_IRQn);
HAL_NVIC_SetPriority(FDCAN1_IT1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(FDCAN1_IT1_IRQn);
/* USER CODE BEGIN FDCAN1_MspInit 1 */
/* USER CODE END FDCAN1_MspInit 1 */
}
}FDCAN_Config function;
/**
* @brief Configures the FDCAN.
* @param None
* @retval None
*/
static void FDCAN_Config(void)
{
FDCAN_FilterTypeDef sFilterConfig;
/* Configure Rx filter */
sFilterConfig.IdType = FDCAN_STANDARD_ID;
sFilterConfig.FilterIndex = 0;
sFilterConfig.FilterType = FDCAN_FILTER_MASK;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
sFilterConfig.FilterID1 = 0x321;
sFilterConfig.FilterID2 = 0x7FF;
if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
{
Error_Handler();
}
/* Configure global filter:
Filter all remote frames with STD and EXT ID
Reject non matching frames with STD ID and EXT ID */
if (HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_REJECT, FDCAN_REJECT, FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE) != HAL_OK)
{
Error_Handler();
}
/* Start the FDCAN module */
if (HAL_FDCAN_Start(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
if (HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK)
{
Error_Handler();
}
if (HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_TX_EVT_FIFO_NEW_DATA, 0) != HAL_OK)
{
Error_Handler();
}
if (HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_TX_EVT_FIFO_FULL, 0) != HAL_OK)
{
Error_Handler();
}
/* Prepare Tx Header */
TxHeader.Identifier = 0x321;
TxHeader.IdType = FDCAN_STANDARD_ID;
TxHeader.TxFrameType = FDCAN_DATA_FRAME;
TxHeader.DataLength = FDCAN_DLC_BYTES_8;
TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
TxHeader.BitRateSwitch = FDCAN_BRS_OFF;
TxHeader.FDFormat = FDCAN_CLASSIC_CAN;
TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
TxHeader.MessageMarker = 0;
}BTW, I removed CAN transceiver from the circuit for testing porpuse.
Here is my test procedure;
I tried to test the GPIO pin (PA11, PA12) with normal Output feature and toggle it. There was no problem with toggling.
When i looked at the CAN RAM section, all the datas were there which i try to send.
And interrupt never occurs.
I also tried to load the example application from the CAN Classic folder but still there was no change.
What should i do to fix this? How can i run the CAN?
2022-09-15 11:26 PM
Thank you so much for your reply Rachel.
You could do this from CubeProgrammer too.
But I did this configuration earlier. Thank you.