cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Pilot communication over direct UART (without ST-LINK) on B-G431B-ESC1

Sujibarathi123
Associate II

Hello ST Team,

I am working with the B-G431B-ESC1 board using STM32G431CBU6 and the STM32 Motor Control SDK.

On the evaluation board, Motor Pilot communicates with the target MCU through the on-board ST-LINK (STM32F103) using SWD and VCP.

My question is:

Is it possible to use STM Motor Pilot to communicate directly over UART with the STM32G431 (for example via an external USB-to-TTL adapter), without using the on-board or external ST-LINK?

1 REPLY 1
STuser2
Senior III

It will work i am not sure what is the confusion. You can refer the below start up guide 

STM32 MC Motor Pilot - Start-up guide - stm32mcu

You have to use the USB to TTL adapter, i am just referring the serial part number you can use to connect to motor pilot. FT232RL USB to TTL Serial Adapter Module 5V/3.3V