2023-09-01 06:43 AM - edited 2023-09-04 12:49 AM
I just noticed the following:
In the datasheets for the G473 and G483 the pin table and alternate function table disagree which pin has the I2C2_SMBA and I2C2_SDA function.
The pin table claims PA10 is I2C2_SMBA and PA8 is I2C2_SDA. The alternate function table claims PA8 is I2C2_SMBA and PA10 is I2C2_SDA.
From experiments it seems the pin table is correct.
Can someone confirm which is the correct alternate function?
Now that I was comparing both columns: it also seems I2C3_SCL is placed differently in both tables: the pin table has it on PA8, the alternate function table on PA10.
EDIT 2023-09-04: for completeness, because I initially forgot:
Solved! Go to Solution.
2023-09-01 07:18 AM
Hello @Loebl ,
Thank you for bringing this issue to our attention.
I confirm the issue and I reported internally.
Internal ticket number: 137961 (This is an internal tracking number and is not accessible or usable by customers).
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-09-01 06:59 AM - edited 2023-09-01 07:01 AM
Hello @Loebl ,
Thank you for reporting!
I will check this internally
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-09-01 07:00 AM
Hello @Loebl
I confirm the problem of I2C2_SDA and I2C2_SMBA in the G483. But G473, this problem doesn't exist.
For the I2C3_SCL problem, I can confirm it for both G4 models.
Best regards.
II
2023-09-01 07:18 AM
Hello @Loebl ,
Thank you for bringing this issue to our attention.
I confirm the issue and I reported internally.
Internal ticket number: 137961 (This is an internal tracking number and is not accessible or usable by customers).
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-09-04 12:34 AM
Thanks for the fast reply.