Skip to main content
Son, Dong-Seong
Associate III
May 28, 2025
Question

STM32F103VCT6 UART Bootloader Connection Fails with “Error: Activating device: KO

  • May 28, 2025
  • 1 reply
  • 518 views

 

I’m trying to use the built-in system memory bootloader on an STM32F103VCT6 and download firmware over UART with STM32CubeProgrammer, but I can’t get the tool to connect. I always see this error:

 
Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...

My setup and procedure:

  1. Hardware

    • MCU: STM32F103VCT6

    • UART pins:

      • PA9 → TX

      • PA10 → RX

    • BOOT0 pulled high to 3.3 V via jumper

    • USB-TTL adapter wired TX↔RX (crossed) & GND common

  2. Boot into system memory

    1. Set BOOT0 = High (3.3 V)

    2. Press and hold RESET (NRST low)

    3. Release RESET (NRST high) and wait ~1 s

    4. (I then move BOOT0 back to Low before connecting—this seemed necessary to power-cycle the logic)

  3. STM32CubeProgrammer UART settings

    • Port: COM ×× (the USB-TTL adapter)

    • Baud rate: 115200

    • Parity: Even

    • Data bits: 8

    • Stop bits: 1

    • RTS / DTR: both low (no hardware flow control)

  4. What happens

    • My user application is definitely not running (no LEDs, no UART output).

    • I click Connect in CubeProgrammer and after a short delay I get the “Activating device: KO” timeout.

  5. What I’ve already verified

    • When I flash via ST-Link in CubeIDE, the application runs fine and UART1 communicates normally with my PC app.

    • My wiring and serial port settings work for the running application.


Question:
What step or configuration am I missing to get the STM32F103VCT6’s UART bootloader to respond? Are there any additional option-byte settings, timing requirements, or hardware details I should check?

Thank you in advance for any advice!

1 reply

mƎALLEm
ST Technical Moderator
May 28, 2025

Hello,

If you are connecting with CubeProgrammer over STLINK, there is no issue with RDP so no option byte constraint.

I suspect an issue with your hardware especially the USB-UART adapter.

Check if your wiring is correct and you are really using  PA9/PA10 for USART1. Check also using a continuity tester the wiring.

Check also if the adapter is not broken. Do the loopback test by looping back Tx to Rx and see if it transmits/receives well via hyperterminal.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Son, Dong-Seong
Associate III
May 28, 2025

Hello,

Thank you for your feedback.

I only use ST-Link during development and debugging. In my production setup the board is enclosed in a sealed case, so ST-Link cannot be accessed. The only exposed interface is the USB-Mini port via a CP2102 adapter wired to USART1, which is why I’m attempting to use STM32CubeProgrammer over UART.

When I flash the STM32F103VCT6 with ST-Link, USART1 communicates perfectly with my Windows GUI—so the USART1 hardware must be working correctly.

Could you please let me know if there are any additional bootloader or UART settings I might have overlooked, or any other configuration steps I should verify beyond what I originally described?

Thank you!

TDK
May 28, 2025

Did you try the steps suggested by @mƎALLEm ?

There are no secret settings here. Get everything right as you outlined in your post and it should work, barring RDP 2. Putting BOOT0 back to GND is unnecessary.

"If you feel a post has answered your question, please click ""Accept as Solution""."