2025-02-16 06:37 PM - last edited on 2025-02-17 02:14 AM by mƎALLEm
STM32G031Y8Y6TR is now burning some problems would like to consult
Serial port 1 after burning OK, when burning again can not read the MCU situation, help to see what will be the reason, how to solve, thanks a lot.
2025-02-16 08:03 PM
Are you holding BOOT0 high during reset so it enters the bootloader?
Is ground connected between board and UART module?
2025-02-16 11:23 PM
There is ground between the board and the UART module, and the BOOT0 remains at a high level of 5V
2025-02-19 09:39 PM
Please look again ,thanks a lot.
2025-02-20 12:00 AM
5V ??
Perhaps instead of kicking the thread you make your presentation of the issue more clear and compelling?
2025-02-20 05:58 AM
Hey check this out: jonahswain/stm32g0-bootloader: STM32G0 microcontroller bootloader