cancel
Showing results for 
Search instead for 
Did you mean: 

[STM32F769 ]Error: Flash Download failed - ''Cortex-M7''

AlbertC
Associate

Hi all,

 

I used the same setting and the same software, keil uVision5. The only different is use my own board rather than EVB, STM32F769I-EVAL. BTW, I use my own board and STM32 ST-Link utility.

Sometimes I can successfully go to debug mode, but sometimes I can't.

 

My question is why keil uVision5 shows 'Error: Flash Download failed - ''Cortex-M7'''.

 

I had erased first then rebuild finished, the next step is starting debug session. Unlucky, it shows error.

 

May need your support on this issue, thank you.

1 REPLY 1
SofLit
ST Employee

Hello,

You need to check your hardware of your own board. Check the VCAPx pins voltage and compare them to what was stated in the datasheet:

SofLit_0-1714468228535.png

Check also the power supply VDD.

Did you refer to the documentation like AN4661 when you started to design your board (see Figure 24 for reference design)?

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.