2022-05-02 12:17 AM
Since the initial configuration, the communication between Cube and the STM32F769 board has been OK.
As I had a problem with the SDRAM configuration, I tried to solve the GPIO conflicts listed in the IOC.
After a modification (I don't know which one) (I suspect an USB_OTG...), the following message appears when I start a debug session:
Error in final launch sequence.
Failed to execute MI command
target remote localhost:61234
Error message from debugger back end:
Remote communication error: Target
disconnected : communication réinitialisée par
le correspondant (in French)Last log lines are:
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Shutting down...
ExitI tried to rebuild a working previous version but I cannot download it as the link is broken.
Is there a way to repair the connection ?
Thanks for your help
2022-05-30 3:00 AM
Hello,
Please check GPIO relative to debugger connection : SWDIO - PA13 and SWCLK PA14
Regards,
Simon
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.