2018-01-11 2:24 PM
I use CubeF7 1.8.0 and the BSP drivers for SD support. Working (reading and writing files) with SD card is fine.
After initializing SD with:
static void SD_Initialize(void)
{ if (isInitialized == 0) { if (BSP_SD_Init() == MSD_OK) { BSP_SD_ITConfig(); isInitialized = 1; } else {/* wait until the uSD is plugged */
while (BSP_SD_IsDetected() != SD_PRESENT) {} } }}UART5 and UART7 are not usable anymore.
Interrupt does not occur anymore and even a simple
HAL_StatusTypeDef hscs = HAL_UART_Receive(&huart5, rxdata, 10, 0x1000);
ends with HAL_TIMEOUT. (A 2nd board sends a string continously)
I also omitted 4 Bit SD, just for testing.
When I make my SD stuff, i.e. reading a config file and then calling
BSP_SD_DeInit();
UART5 and UART7 can properly used, with IT or without.
UART6 for instance is not affected by the SD functions.
Other UARTs are not accessible with STM32F769-DISCO, so I don't know if they work or not.
The goal is an application with SD, 3x UARTs, STEmWin, Ethernet. Everything works nice except the
combination of SD and UART5/7.
Any idea?
Thank you, Joerg
#uart5 #uart7 #sd #bsp #stm32f769-discoSolved! Go to Solution.
2018-01-12 8:57 AM
To initiate the UART reading via Interrupt you have to clear Overrun and Timeout flag
if incoming data fills up the receiver:
__HAL_UART_CLEAR_IT(&huart7, UART_CLEAR_OREF|UART_CLEAR_NEF|UART_CLEAR_RTOF);
HAL_UART_Receive_IT(&huart7, &rx7_ch, 1);__HAL_UART_CLEAR_IT(&huart5, UART_CLEAR_OREF|UART_CLEAR_NEF|UART_CLEAR_RTOF);
HAL_UART_Receive_IT(&huart5, &rx5_ch, 1);There is no relationship between SD and UART functions. Side-effect.
2018-01-11 3:31 PM
NVIC Interrupt Grouping and Preemption?
Mindless blocking in interrupt/callback routines?
With HAL you really want SysTick to preempt everything
Next level down USART, service and leave.
If the SDIO/SDMMC is simply flagging completion, or error, it doesn't need to preempt more time critical code.
2018-01-11 5:25 PM
,
,
Hi Clive.
I use no FreeRTOS and using a plain
HAL_StatusTypeDef , hscs = HAL_UART_Receive(&,huart5, rxdata, 10, waiting),
returns with a HAL_TIMEOUT, no interrupts are used in this case.
Baudrate is 4800 only!
When I initiate the mechanism with
, , , HAL_UART_Receive_IT(&,huart7, &,rx7_ch, 1),
,
, , ,HAL_UART_Receive_IT(&,huart6, &,rx6_ch, 1),,
, , ,HAL_UART_Receive_IT(&,huart5, &,rx5_ch, 1),it works with interrupts unless SD is activated. Priorities of SD and UART Interrupts are different.
Pins of UARTs:
♯ define UART5_RX_Pin GPIO_PIN_9
,
♯ define UART5_RX_GPIO_Port GPIOB,
♯ define UART5_TX_Pin GPIO_PIN_8,
♯ define UART5_TX_GPIO_Port GPIOB♯ define UART7_RX_Pin GPIO_PIN_6
,
♯ define UART7_RX_GPIO_Port GPIOF,
♯ define UART7_TX_Pin GPIO_PIN_7,
♯ define UART7_TX_GPIO_Port GPIOFThere is no collision with SD pins noticeable.
No SD=No Problems
2018-01-11 6:12 PM
Does it corrupt the data, do the USART give an overrun or framing type error, or just time out?
If things are timing out it is indicative of some blocking code, perhaps in interrupt context (ie call back, theirs or yours)
Assume 0x1000 is around 4 seconds, so should be enough time, wouldn't expect SD code to block for that long unless reads/write are being chained endlessly, or the SD card traffic is being generated in an interrupt.
Not sure there are any design conflicts that would cause the hardware not to function properly.
2018-01-12 1:12 AM
HAL_TIMEOUT
You can set the waiting time to an hour theoretically and you will wait this time.
Both UARTs are not working properly after SD initialization. It's not neccessary
to mount and read form a SD card. It's the SD init function of the BSP.
When creating a tiny project with CubeMX enabling SDMMC and FatFS with INT
but without DMA usage, it does not corrupt the UART's. (UART's do not use DMA)
For my project it's not a must to use both resources (SD and UART's) at the same
time. Until I don't know the reason I will read my data from the UART's, activate the SD IP,
write the data into a file and disable SD with
BSP_SD_DeInit();
to get the next data from the UART's.
Turning it on and off is not the solution, but better than nothing.
2018-01-12 8:57 AM
To initiate the UART reading via Interrupt you have to clear Overrun and Timeout flag
if incoming data fills up the receiver:
__HAL_UART_CLEAR_IT(&huart7, UART_CLEAR_OREF|UART_CLEAR_NEF|UART_CLEAR_RTOF);
HAL_UART_Receive_IT(&huart7, &rx7_ch, 1);__HAL_UART_CLEAR_IT(&huart5, UART_CLEAR_OREF|UART_CLEAR_NEF|UART_CLEAR_RTOF);
HAL_UART_Receive_IT(&huart5, &rx5_ch, 1);There is no relationship between SD and UART functions. Side-effect.