2016-06-28 12:51 AM
Hi, I have a problem with my stm32f46g disco board. When I want to compile program on mbed.org and after that copy that file to disco board I get a fail.txt and info: RESERVED BITS. What happen? I may connect with ST-Link, its connects without problem.
09:48:33 : ST-LINK SN : 066AFF525053885087033137
09:48:33 : ST-LINK Firmware version : V2J23M7 09:48:33 : Connected via SWD. 09:48:33 : SWD Frequency = 1,8 MHz. 09:48:33 : Connection mode : Normal. 09:48:33 : Device ID:0x449 09:48:33 : Device family :STM32F7xx2016-06-29 04:04 AM
Hi karol.karol,
May be you can get more help about this issue in forum -Syrine-2016-06-29 04:33 AM
Or perhaps start by getting the most current firmware on the ST-LINK?