cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f746 ETHERNET issue

clock.1166
Senior

Hi,

Could anyone help with this problem? Its driving me mad!!!

I have designed an ethernet interface  for an F746-100 MCU

I have changed pins to avoid using Port G and I have used the  circuit below.

The RJ45 connector is a standard RB1-125BAG1A and the ethernet chip is a LAN8742A

Can anyone tell me if there are any mistakes in this?

I cannot get any connection at all - F746-100 will not ping.

Green LED ON and Yellow LED flashes continuously.

I have an STM32F746 - 144 Nucleo with the same software (apart from the two pins that are changed) -works fine.

The 25MHz xtal works OK (same signal on both boards) and the LAN8742_STATUS_OK returns 0  on both boards when I debug.

There appears to be no errors in the setup LAN8742.c or the ethernetif.c when I debug. This code works OK on the NUCLEO board and I can display a small webpage. Both sets of code use only ETH and LWIP, fixed IP, on a standard Cubeide setup. I assume that the only difference is the two GPIO allocations (PG13>PB12 and PG11>PB11) which I have altered in software.

I have the same sort of signals on both boards on TXP/TXN/RXP/RXN

Can some kind soul tell me if there is anything obviously wrong with my hardware?

Thanks.

Chris

1 ACCEPTED SOLUTION

Accepted Solutions
clock.1166
Senior

JOY of JOYS!!!

A *** mistake -

4 resistors on Ethernet circuitry were incorrect.
I am not too familiar with SMD markings, and I wrongly assumed '4992' was 49.9 ohms, when in fact they are 49.9Kohms.
It was not possible to measure them on the board since they were across a coil.
I replaced them with 4 standard resistors and ethernet works OK!

Thank you all so much for helping me.

The circuit and the project I uploaded are guaranteed to work, so hopefully this will help others.

Chris

image.png

  

View solution in original post

21 REPLIES 21
STOne-32
ST Employee

Hi @clock.1166 ,

 

Here are few hypothesis :

  • Check the clocks of the PHY and also the signals going to the LQFP100 leads ( I have seen in the past some surprises)
  • re-check if PB11 and PB12 are not reconfigured somehow in Software to other functions than Ethernet . It is strange that a debug all is working from you side .
  • may be a signal integrity matter  if all TX signals are coming correctly to the PHY with the Ref Clock , may be to check the driving level of these I/O setting by software- I/O speed .

Hope it helps you .

Cheers,

STOne-32

clock.1166
Senior

Thanks for your help STOne, but I have checked the software and I cant find anything amiss. The clock (25Mhz) and reference (50Mhz) are identical to the NUCLEO F746, and so are the TXP/TXN/RXP/RXN as far as I can ascertain.

I've tried running the board at a lower main clock speed, but how do you set the I/O speed as you've mentioned?

I just wish there was a simple ETH+LWIP project around for an F746 LQFP-100. I haven't managed to find one.

I also cannot understand what the flashing yellow LED means - any ideas?

I am not an expert in high frequency design and I am struggling!

Chris

Setting I/O speed is done when the port B is configured to Alternate function and should be in Output speed parameter if you can share your Ports settings versus Our LQFP144 Nucleo code software . 

Let us know,

STOne-32

clock.1166
Senior

One interesting thing: If I completely erase the STM32F746-100, the Leds act in exactly the same fashion when the port is connected to the router.

Green LED ON and Yellow LED flashes continuously.

Can I deduce anything from that?

Thanks.

Chris

May be to double check the PHY configuration and signals on the  PCB to the RJ45 Connector. Not sure what is the cause here .  @STea  your help is appreciated

ciao

STOne-32

STea
ST Employee

Hello @clock.1166 ,

Implementing the Ethernet on custom board can be a challenging task and i will try to help you to get over this problem .

first i need some clarification with previous conversation with @STOne-32 . 

  1. "The 25MHz xtal works OK (same signal on both boards) and the LAN8742_STATUS_OK returns 0  on both boards when I debug." how did you make sure that the Xtal 25 Mhz is outputting the same signal on both boards i ask you this because issue with the precision of the clock source can lead the application to malfunction.and the jitter can affect the Ethernet periph behavior.
  2.  is the gpio speed for all the assigned pins is put to very high this is also the recommended setting for the Ethernet ?

adding on that i have to ask you some further questions to verify the root cause of this problem:

  1. verify if there is a change in the VDD level between the two boards .
  2. check if you can visualize the signals from the TXD0 and TXD1 to see if there is traffic between the MCU and the LAN8742A
  3. try to read the status of  LAN8742A with the help of the init function api in LAN8742.c in run mode (toggle an LED when LAN8742_STATUS_OK returns 0 )
  4. the RST pin in your design seems to be not connected can you give more info on it its not clear in the picture 
  5. can you give us information about the clock source feed to the MCU .

hope you will get back to me with some good news or helpful information to get it working soon.

BR

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
clock.1166
Senior

Thanks STea/Stone-32,

I have placed (I hope) a better image of my circuit. Any suggestions would be helpful!

I have a feeling that this is the source of all my problems, although I dont know enough about LWIP and ETH to be certain.

I cannot find any similar project using STM32F746-100. It would be helpful if I could.

 

1. I compared the clocks from an STM32F746 nucleo (which works fine with the same basic software) to my board with a scope. The reference clock(50Mhz) and the xtal clock (25Mhz) looked almost exactly the same - 25.010 and 25.1 MHz - same amplitude. The signals on TXP/TXN/RXP/RXN also  look the same.

2. Yes -  GPIO's set to very high.

Simple webserver for Nucleo F746 generated from cube IDE attached (http://192.168.1.218/)

F746-100 generated same way - obviously ETH pins are slightly different.

I will work on the other questions today.

Thanks.

LCE
Principal

25.1 MHz - that on the board that is not working?

50 MHz clock is generated by the PHY?

After your GPIO switch - checked all the alternate function numbers?

PCB layout: around the crystal and clocks all clean? No crazy routing of the high speed signals?

PHY: Read all the registers and check / compare to datasheet.

clock.1166
Senior

Screenshot 2024-01-30 103317.png

 Possibly slightly better image?