cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F722VET6 MCU Malfunctioning

SPate.14
Associate

We are using STM32F722VET6 MCU in one of our project.

Memory defined are in linker as below:

RAM : 256KB

ROM : 512KB

Stack : 4KB

We have configured below peripherals and developed an application code using user defined functions. Which is working as expected.

• UART1, UART2

• SPI1, SPI2, SPI3

• GPIO`s

But when we define few more functions and call them then the application behaves abnormally, below are our observations.

• We are able to compile & download the code (using ST-LINK) but when we execute the code it malfunctions. 

• Most of the global variables defined with some constant values shows the garbage/null characters in debug mode

We have created a sample code using STM32CubeMX and integrated our application code in it. But unfortunately, this also gives the same problem.

Please find attached screenshots of Flash & RAM consumed by our application and Linker file for Stack, heap, RAM & Flash memory assignment.

2 REPLIES 2
T J
Lead

First things I would check and shutdown to become stable...

can you check the power rails ? or is it a nucleo board ?

can you check the VCap pins?

is Boot0 held low or floating ?

turn off the Cache

increase the heap

set debug to -o0 and set a break point in the hardfault.

when it becomes unstable pause and check your hardware registers.

Usually a run away buffer pointer is the cause, and crap is being written into registers..

Assuming it is a software problem you'll need to put your developer pants on and debug the situation.

Instrument the code so you can determine the flow and interactions in the code and evolve your understanding of the issue beyond "not working".​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..