2023-03-20 08:08 AM
Hello,
I want to use the X-Cube STL on the STM32F722RET7 and have the problem that the STL_SCH_Init () function returns STL_KO (an error).
The user manual says that this is due to defensive programming in the STL. Unfortunate the STL is precompiled and no debugging is possible.
Does anyone know if there are some preconditions that must be considered for running the STL?
Thank you very much.
2023-03-22 07:08 AM
Please contact you local FAE and raise an official support request, this FW is under NDA and this public forum is not good platform to discuss possible solutions.
Thank you for understanding.
Best regards,
Petr