2017-09-18 09:20 AM
I have noticed that STM32F7 microcontroller generates a digital noise (see the figures. It is not from transmission lines and bursts are repeating every 16ms) on the 5.0V supply voltage.
I have observed this using both Discovery and Nucleo boards.
I have seen this using external power supply and the power over USB.
I have also tried different sample codes. It actually does not matter what code you run, because even before I start the code in my debugger, the ripples can be observed. The only time, I do not see the ripples, is when the microcontroller is kept in reset, or when I remove a jumper to power it down.
I have also noticed that, after couple of resets, the noise sometimes disappear. It comes back if I reset again.
Anyone else who has observed this issue? Any thoughts?
#ripples #noise #stm32f7 #power-supply2017-11-28 03:00 PM
SDRAM specs
Alliance :- AS4C8M16SA
128M - 8M x 16 bit Synchronous DRAM (SDRAM)ï‚· Auto Refresh and Self Refresh
ï‚· 4096 refresh cycles/64msMicron:
• PC100- and PC133-compliant
• Auto precharge, includes concurrent auto prechargeand auto refresh modes• Self refresh mode (not available on AT devices)• Auto refresh– 64ms, 8192-cycle (commercial and industrial)– 16ms, 8192-cycle (automotive)• LVTTL-compatible inputs and outputs• Single +3.3V ±0.3V power supplythere is your 16mS noise...
2017-11-28 06:03 PM
looks like bad decoupling on memory chips