2021-04-13 4:54 AM
Hello ST,
From datasheet(PM0253),
The SHPR1-SHPR3 registers set the priority level, 0 to 255 of the exception handlers that have configurable priority.
Also from datasheet,
Each PRI_n field is 8 bits wide, but the processor implements only bits[7:M] of each field, and bits[M-1:0] read as zero and ignore writes.
What is the value of M? How does this relate to Binary point priority grouping?
Thanks
Dheeraj
Solved! Go to Solution.
2021-04-14 1:54 AM
I got the answer for this. The value of M depends on the value of priGroup set in AIRCR register. The range is described in Priority Grouping table 56. For example, if PRIGROUP is 0b001, M is 2.
2021-04-14 1:54 AM
I got the answer for this. The value of M depends on the value of priGroup set in AIRCR register. The range is described in Priority Grouping table 56. For example, if PRIGROUP is 0b001, M is 2.