cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4x: Need help to use Flash file system on SPI based NAND Flash

Vikas Nandwani
Associate
Posted on May 22, 2018 at 14:31

Hello, I am new user of STM32F4x. I am looking for some help in using a flash file system on SPI based NAND Flash. Are there any examples or demonstrations that I can look for to start with?

A  demo that makes use of part of on chip flash memory as a disk also would be useful.

I have STM 

Discovery kit with STM32F429ZI MCU (

http://www.st.com/en/evaluation-tools/32f429idiscovery.html

)

#stm32f4 #stm32f4-flash-mem
1 REPLY 1
Posted on May 22, 2018 at 16:26

>>I have discovery evaluation board 

You're going to have to be a bit more specific. Write the full name, or link to the webpage.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..