2018-05-22 5:31 AM
Hello, I am new user of STM32F4x. I am looking for some help in using a flash file system on SPI based NAND Flash. Are there any examples or demonstrations that I can look for to start with?
A demo that makes use of part of on chip flash memory as a disk also would be useful.
I have STM
Discovery kit with STM32F429ZI MCU (
)#stm32f4 #stm32f4-flash-mem2018-05-22 7:26 AM
>>I have discovery evaluation board
You're going to have to be a bit more specific. Write the full name, or link to the webpage.