STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103 - CubeMX DFU

Hi,I couldn't find online a working bootloader implementation of STM32f103C8 based on generated files from CubeMX, i've started porting the F4 DFU to F1, there are two applications: 0x08000000 - DFU Bootloader0x08008000 - ApplicationJump between the ...

Resolved! Another funny typo, in the USART chapters of RMs

In USART block diagram figure, "f" in "Transmit shift register" is missing, giving it a whole lot different meaning... ;)Besides this, the arrows from both "shi(f)t registers" to their respective data registers have incorrect direction. The LPUART ch...

Help with X-CUBE-SPN2 for IHM02A1

Posted on December 01, 2017 at 21:47Has anyone used the IHM02A1 and got either the project files or the pre-compiled binary and hex files to work? If so, could you please tell me if you did anything to get them to work or did they simply work out of...

DMA multi-using problem

Posted on October 24, 2017 at 11:30I use STM32F103, DMA1->CH6USART2 RX and TIM3 TIM3_CH1 both can use this channel.If only USART2 RX or TIM3 TIM3_CH1 to use this channel,it is ok!but how to multi use for two request?thank you very much.

STM32F030C8T6 DMA USART CHANNEL REMAPPING QUESTION

Hi everyone: As a title,I use dma Usart Rx for DMA1 Channel 3,but at the same time, I also use Spi Tx for DMA.So , I must remap Usart Rx from DMA1 Channel 3 to DMA1 Channel 5.I try to use this function SYSCFG_DMAChannelRemapConfig(SYSCFG_CFGR1_USAR...

Help required with porting from STM32F767ZI to STM32F779NI

I have code that runs on the NUCLEO-F767ZI kit and have recently obtained the STM32F7779I-EVAL kit. My program is very simple, it does not do any IO (yet), so I (perhaps naively) thought that just changing the processor type in my IAR Embedded Workbe...

KDuff.15 by Associate II
  • 1456 Views
  • 2 replies
  • 0 kudos