2013-01-22 3:39 AM
I need to use I2C1 ports for communication with LG3D20(0xD6 adress) gyro sensor.Accordingly, i need i2c1 initial,i2c1 write data 1 byte,i2c1 read data 1 byte functions.I am using these functions but i couldnt run this function in program flow.The program always lockups at I2C_GetFlagStatus(I2C2, I2C_FLAG_BUSY).Please give me an tried example for stm32f4discovery i2c1.My codes are here:
/* I2C1 */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); GPIO_PinAFConfig(GPIOB,GPIO_PinSource6, GPIO_AF_I2C1); GPIO_PinAFConfig(GPIOB,GPIO_PinSource7, GPIO_AF_I2C1); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_Init(GPIOB, &GPIO_InitStructure);I2C_DeInit(I2C1); RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE); I2C_init.I2C_Mode = I2C_Mode_I2C; I2C_init.I2C_ClockSpeed = 100000; I2C_init.I2C_DutyCycle = I2C_DutyCycle_2; I2C_init.I2C_OwnAddress1 = 0; I2C_init.I2C_Ack = I2C_Ack_Enable; I2C_init.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_Cmd(I2C1,ENABLE); I2C_Init(I2C1,&I2C_init); unsigned short int I2C1_read(uint8_t adress, uint8_t index) { uint8_t data; while (I2C_GetFlagStatus(I2C1, I2C_FLAG_BUSY)); I2C_GenerateSTART(I2C1, ENABLE); while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); I2C_Send7bitAddress(I2C1, adress, I2C_Direction_Transmitter); while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); I2C_SendData(I2C1, index); while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); I2C_GenerateSTART(I2C1, ENABLE); while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); I2C_Send7bitAddress(I2C1, adress, I2C_Direction_Receiver); while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED)); while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_RECEIVED)); data=I2C_ReceiveData(I2C1); I2C_GenerateSTOP(I2C1, ENABLE); return data; } void I2C1_write(uint8_t adress, uint8_t * data) { uint8_t i=0; while (i < 7) { while (I2C_GetFlagStatus(I2C1, I2C_FLAG_BUSY)); I2C_GenerateSTART(I2C1, ENABLE); while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); I2C_Send7bitAddress(I2C1, adress, I2C_Direction_Transmitter); while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); I2C_SendData(I2C1, data[i]); while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); I2C_SendData(I2C1,i + 1); while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); I2C_GenerateSTOP(I2C2, ENABLE); i+=2; } }int main(void){ uint8_t timer_value,flag=0,i=0; char buffer[8]; uint8_t deger; I2C1_Initialize(); while (1) { deger=I2C2_read(0x3C,0x20); sprintf(buffer,''%d'',deger); USART3_Write_Text(buffer); USART3_Write_Text(''\n\r''); }}I need read,write,initial functions for stm32f4discovery kit's I2C1!!! #stm32f4discovery-i2c1-problem!!!