2024-05-04 10:24 PM
I need to download the STM32F4DISCOVERY board firmware package for the MATLAB toolbox, but it's not available for download on the official website.
2024-05-05 12:01 AM - edited 2024-05-05 12:01 AM
Hello @oleehu and welcome to the ST Community :smiling_face_with_smiling_eyes:.
For such a firmware package, i suggest you to the Mathworks website.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-05 5:02 AM
But MathWorks doesn't provide download packages, the download link on the MathWorks website redirects to the ST official website.
2024-05-05 6:02 AM
As I recollect support for the STM32's was integrated into MatLab at some point. MIL? (Micro-processor In the Loop)
There was like one guy at ST that supported the original effort. You'd do better checking in the MatLab orientated forums, than here.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.