2019-09-17 12:29 AM
hello. i can see 500K Bps on CAN1 and i can't see this baud rate on CAN2. I use same bit timing and i can't see this baud rate. What is the maximum baud rate limit on CAN2? I attached source folders. I am waiting answer as soon as possible. Best regards.
2019-09-17 2:42 AM
The clock comes from the same APB source, the prescaler and quanta settings control the wire speed.
2019-09-17 3:36 AM
I do not understand. Can you explain in more detail