2019-02-04 5:31 AM
STM32F446ZET6 FMC: Are FMC_NCE3 and FMC_NE2 signals connected to only one PIN PG9? Or that is documentation bag?
2019-02-04 7:58 AM
Hello,
The datasheet is correct: FMC_NCE3 and FMC_NE2 signals are connected to PG9 pin.
Kind Regards,
Imen
2019-02-04 8:15 AM
Thank you! The same is written in other documents. But why they are combined. This makes it difficult to RAM-NAND memory expand