STM32f429zi usart interrupts
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-07 5:32 AM
Hi guys hope you are doing well, I am having some issues generating a USART Interrupt to receive data in my project using the Standard Peripheral Library not HAL...I wanted to ask if there is someone who might have a simple code based on usart interrupts, my code here
- Labels:
-
Interrupt
-
STM32F4 Series
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-07 8:10 AM
if(USART_GetITStatus(USART3, USART_IT_RXNE) != RESET){
USART_ClearFlag(USART3, USART_FLAG_RXNE); // <<<< Don't need this, the read will implicitly clear the status/interrupt
rxByte = USART_ReceiveData(USART3);
Should perhaps also have code to check parity, framing, noise error and clear those.
Does transmit work? Check HSE_VALUE setting
// STM32 USART IRQ TX/RX Loop (USART3 Tx PD.8, Rx PD.9) STM32F4 Discovery - sourcer32@gmail.com
#include "stm32f4_discovery.h"
volatile char StringLoop[] = "The quick brown fox jumps over the lazy dog\r\n";
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* USART3 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);
/* GPIOD clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOD, &GPIO_InitStructure);
/* Connect USART pins to AF */
GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_USART3);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_USART3);
}
/**************************************************************************************/
void USART3_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
/* USARTx configuration ------------------------------------------------------*/
/* USARTx configured as follow:
- BaudRate = 9600 baud
- Word Length = 8 Bits
- Two Stop Bit
- Odd parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART3, &USART_InitStructure);
USART_Cmd(USART3, ENABLE);
USART_ITConfig(USART3, USART_IT_RXNE | USART_IT_TXE, ENABLE);
}
/**************************************************************************************/
void NVIC_Configuration(void)
{
NVIC_InitTypeDef NVIC_InitStructure;
/* Configure the NVIC Preemption Priority Bits */
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0);
/* Enable the USART3 Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = USART3_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
/**************************************************************************************/
void USART3_IRQHandler(void)
{
static int tx_index = 0;
static int rx_index = 0;
if (USART_GetITStatus(USART3, USART_IT_TXE) != RESET) // Transmit the string in a loop
{
USART_SendData(USART3, StringLoop[tx_index++]);
if (tx_index >= (sizeof(StringLoop) - 1))
tx_index = 0;
}
if (USART_GetITStatus(USART3, USART_IT_RXNE) != RESET) // Received characters modify string
{
StringLoop[rx_index++] = USART_ReceiveData(USART3);
if (rx_index >= (sizeof(StringLoop) - 1))
rx_index = 0;
}
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
NVIC_Configuration();
USART3_Configuration();
while(1); // Don't want to exit
}
/**************************************************************************************/
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* Infinite loop */
while (1)
{
}
}
#endif
/**************************************************************************************/
Up vote any posts that you find helpful, it shows what's working..