2024-02-05 4:00 PM
Hi.
I was in the middle of a debug session in a simple application for the STM32F429I-DISC1 in Keil uVision. I disconnected my board from the computer without ending the debugging session. When I reconnected my board, it wasn't detected anymore and it enters debug mode (I know it because the LED1 blinks) as soon as I connect it. Now I can't flash or debug anything.
Anyone can help?
Solved! Go to Solution.
2024-02-15 12:20 PM
Hello everyone. Thank you to those of you who have answered my question. The issue solved itself. I reconnected the board the next day I was having the issue and it worked fine. It was a little weird as I tried to reconnect the board several times and it wasn't working. Luckily, it seems I just had to wait longer to reconnect the board.
2024-02-05 5:16 PM
You're going to have to go deeper into the circumstances, what were you doing? What else was connected to the board? Was it on a non-conductive surface?
Sounds like you damaged the board electrically.
2024-02-05 5:42 PM
LD1 blinking suggests ST-Link isn't connecting. Try rebooting.
For what it's worth, disconnecting the board without ending the debug session will not damage anything.
See if STM32CubeProgrammer can detect the ST-Link and connect.
2024-02-15 12:20 PM
Hello everyone. Thank you to those of you who have answered my question. The issue solved itself. I reconnected the board the next day I was having the issue and it worked fine. It was a little weird as I tried to reconnect the board several times and it wasn't working. Luckily, it seems I just had to wait longer to reconnect the board.