2018-04-26 8:16 AM
Hello,
i am using a design with a STM32F427 100pin package, and notice after leaving the board unpowered for several hours if i power up again, the software its not starting.
If i retry the restat the power it will stil not work, only after 3-4 retries.
If i have the change to get starting the software, then if i power off/on it still works.
Boot1 - pin is left floating
Boot0 pin - is tied to ground trough a 4K7 resistor
Reset pin - is tied to 3.3V trough 4k7 resistor.
Capacitors from pins 49,73 ( V_CAP) are 100nf X7R smd type
What is causing this strange behaviour?
2018-04-26 8:35 AM
Analog supply/ground pins not connected?
Software issue?
JW
2018-04-26 11:16 AM
Sure it is not starting?
Try adding an effective POR circuit (MCP120 type device with >100ms clamping of NRST)
Add code tight into Reset_Handler to provide signs of life immediately, before it gets stuck in loops waiting for HSE, PLL, etc to spin up.
Make sure Hard Fault reports.
2018-04-26 12:10 PM
The power supply pins are all connected, the ground pins the same.
I am wondering if this is a software issue, since once the software starts everything seems to work perfectly.
2018-04-26 4:44 PM
Definitely sounds like a Reset Issue.
this is my solution, I never have startup issues.
2018-04-26 4:48 PM
Honestly i work with stm32f4 as a hobby for some years now, and never used dedicated POR ic for thss, never had such problems like this.
Also each power pin is bufferd by a 1uf tantal cap
I wil double check the resistor on the reset pin, is there any typical value for this?
2018-04-26 7:06 PM
Do you have a weak power supply ?
if the Vdd rail is slow to come up, this will
exacerbate
the reset issues.Do you have a scope ?
you could trigger on the reset pulse going high, but check the rails ramping up time.
The Reset pin needs a resistor and a Cap.
You mentioned the 4k7, but you didn't mention the cap.
I use a 10k pullup and a 0.1uF on the reset pin as a minimum, but its not 100% reliable, depending on the brown out duration.
For 100% reliable startup, use the reset chip.
2018-04-27 12:14 AM
Could be a temperature-related clock problem as well.
You could try to heat it up after a long power off, before turning on.
If the startup problems are gone, I would check the clock setup and timings.
Power supply circuitry could create the same symptoms, but IMHO less likely.
2018-04-27 7:27 AM
Hello,
Bellow is a scope image, yellow is the 3.3V supply line, and purple is the reset pin.
The measurements where taken at 500uS/1V division.
I dont have capacitor on the reset pin
What do you think?
2018-04-27 7:06 PM
I would say you definitely need a cap, is that 1uSec from power supply at 2.5v to Reset up ?
did you check the reference manual ?
page 29 of the F427 data sheet, VACAP has to be stable before Reset, can you check that ?
you should check pages 25-29
Page 97, NRST Pin
page 138: You need a 0.1uF, and no resistor ??
Table 59. NRST pin characteristics shows:
Time of NRST_OUT Generated reset pulse duration Internal Reset source 20 - - μs
I can't see this 20uS running on your scope.
page 222
Appendix A Recommendations when using internal reset OFF