2015-12-01 08:27 AM
Hi !
I'm just wondering if anybody have seen similar behaviour with LSE on revision ''1'' silicon of STM32F4107VG6.LSE starts perfectly at room temp but fails to start completely at temps below -15 celsius.Load capacitors and oscillator selection was done strictly according to application note.We started experience this behaviour on silicon revision ''1'' chips. On previous silicon revision ''Z'' everything was ok.BR,Oleg2015-12-01 08:32 AM
2015-12-01 10:12 AM
The STM32 parts are very sensitive to the characteristics/gain of the LSE component/circuit implementation. It can result in very slow starting, or non-starting of the crystal, but this should be demonstrably different from it not executing any code. ie you should be able to output diagnostics via a USART or GPIO/LED, to identify it is running normally, and then attempting to start the LSE. Neither crystal is started automatically, which makes signs-of-life testing of free standing STM32 quite difficult.