2015-11-30 9:26 PM
Hi,
I've got all documentation for the STM32L4 Discovery board (and I have a board too) and want to remove the LCD screen to free up some I/O for some ADC inputs. I am trying to use the CubeMX tool to help with this. I've selected the board in the configuration. It shows ADC1,2 and 3 as not available (used up by this, that and everything else) For example, if I wanted to (physically) remove the LCD and use PC3 on ADC1, how do I convince CubeMx I really want to do this? I mean, it just won't let me. Or can CubeMx not be used this way? The ST video on the Discovery board seems to assure the user that the I/O can be used if the LCD is removed, but CubeMx doesn't seem to let the user have them. Thanks for any help on this! #stm32l4-adc-cubemx2015-12-01 10:42 AM
Just tell CubeMx you have a STM32L476VGT6
PC3 is connected to VLCD circuitry that doesn't go away when you remove the LCD. My recommendation: get a NUCLEO-L476RG to experiment with ADC programming. Cheers, Hal2015-12-01 11:06 AM
thank you for answering, baird.hal.001
Looks great - CubeMx looks like it will let me use and configure all the ADC's I need.