2017-10-18 1:31 AM
Hi All,
I tried to use USART6 but the data I sended is corrupted, I check the baudRate bur its looks fine(9600 bps), I add the screen shot of oscilloscope I send 0x79(0b0111 1001) but its showed me irrelevant data, also I tired the diffrent baudrate but result was same,
Here is my USART6 initialization code;GPIO_InitTypeDef GPIO_InitStruct;
USART_InitTypeDef USART_InitStr; RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART6, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_USART6); GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_USART6); GPIO_InitStruct.GPIO_OType = GPIO_OType_PP; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStruct.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_100MHz; GPIO_Init(GPIOC, &GPIO_InitStruct); USART_InitStr.USART_BaudRate = 9600; USART_InitStr.USART_WordLength = USART_WordLength_8b; USART_InitStr.USART_StopBits = USART_StopBits_1; USART_InitStr.USART_Parity = USART_Parity_No; USART_InitStr.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStr.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART6, &USART_InitStr);USART_Cmd(USART6, ENABLE);I send with, USART_SendData(USART6, 0x79);
The response I read on terminal 0b1111 1001(Dec: 159)(Hx: F9)
Thanks in advanced.
Yigit
2017-10-18 5:26 AM
I guess some bits is missing, it could be stopbit but why is the stopbit missing?
Dunno, perhaps the Serial/USB converter does not support all settings.
I would check a 0xAA and 0x55 pattern, with a scope.
And I'm still not sure if the settings for your PC terminal application are correct.
TX(F407) RX(TeraTerm)
0b
01
11 1001 ------------------------------------> 0b11
11 10010b
01
00 0111------------------------------------>
0b10
00 01110b
01
01 0100----------------------------------->
0b10
01 0100Rather looks like a problem with the first bits.
2017-10-18 5:27 AM
Read out and post the RCC and UART registers content.
JW
2017-10-18 6:13 AM
Unsurprisingly, this settings seem to match those of the F407.
But what stands out, at least for me :
GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP;
I initialized this pins always with GPIO_PuPd_NOPULL, which worked for me.
2017-10-18 6:45 AM
I don't see an immediate problem with the clock settings.
And according to my experience, a core clock mismatch looks different.
You receive just garbage, not at all resembling the sent values.
What is suspicious - PC7 is connected to the MCLK input of the audio codec (CS43L22).
There seems no alternative route for UART6 RX - have you tried another UART ?
2017-10-18 7:04 AM
it is happen beacuse of 'HSE_VALUE' symbolic constant it was not equal to actual crystal value, how I forgot the fix it,
Can you tell us the difference between the specified and the actual value ?
The 'usual' case was 25 MHz instead of 8 MHz when using the SPL (default quartz on ST eval boards vs. ST disco boards).
And that looked >>very<< different.
Your freqencies must have been quite close.
2017-10-18 7:17 AM
Hello!
Inside stm32f4xx.h the default HSE value is 25000000
Discovery's crystal is 8000000 Hz
2017-10-19 1:39 AM
Hi, the problem is with your RS232 analyzer: the oscilloscope image you attached shows a perfect 0x79.
- serial comm starts with a start bit (the first low level part before point 'a')
- then 8 bit data starting with the least sigificant bit (0x79= 0111 1001,but in order it is 10011110)
- parity bit (if enabled)
- stop bit (H level)
- idle (H level) if no immediate next byte
So the sequence you need to see (in real order) is:
0(start bit) - 10011110 (data, LSB first) - 0(parity bit) - 1(stopbit)
(you can't really see stop bit, as it is the same level as the idle following)
Check your recording, everything fine.
2017-10-19 3:52 AM
I mean sorry I didn't noticed that parity is disabled in your initialization code. Oscillogram shows the good 0x79 but with parity.
One more thing: a-b time is 109.9usec. Exact bit time is 104.2usec, so this 5.5% difference may corrupt communication if the receiver side also has a difference in the opposite direction.
I'd measure a longer period for higher accuracy: from the first H->L edge (start of startbit) to the last L->H (start of stopbit) it should be 9 (witohut parity) or 10 (paritiy enabled) bit times, so 937.5 or 1041.7 usec.
2017-10-19 3:52 AM
That would be right, but at 9216Baud, not at 9600.
The problem is in timing, i.e. in clocking of the USART, and possibly the whole mcu.
JW
2017-10-19 4:13 AM
Sorry Jan, I didn't check all the posts.
Anyway the whole case doesn't fit: the oscillogram seems a 9600bps comm with parity and a slighty differing clock. Its bit time is surely not shrinked or widened by 8/25x or 25/8x ratio ...
Okay, I see case is closed, gotta leave it:)))