cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407 - USART6 Tx Frame Error

ygt_1108
Associate II
Posted on October 18, 2017 at 10:31

Hi All,

I tried to use USART6 but the data I sended is corrupted, I check the baudRate bur its looks fine(9600 bps), I add the screen shot of oscilloscope I send 0x79(0b0111 1001) but its showed me irrelevant data, also I tired the diffrent baudrate but result was same,

Here is my USART6 initialization code;

GPIO_InitTypeDef GPIO_InitStruct;

USART_InitTypeDef USART_InitStr;

RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART6, ENABLE);

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);

GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_USART6);

GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_USART6);

GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;

GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP;

GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStruct.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;

GPIO_InitStruct.GPIO_Speed = GPIO_Speed_100MHz;

GPIO_Init(GPIOC, &GPIO_InitStruct);

USART_InitStr.USART_BaudRate = 9600;

USART_InitStr.USART_WordLength = USART_WordLength_8b;

USART_InitStr.USART_StopBits = USART_StopBits_1;

USART_InitStr.USART_Parity = USART_Parity_No;

USART_InitStr.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

USART_InitStr.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

USART_Init(USART6, &USART_InitStr);

USART_Cmd(USART6, ENABLE);

I send with, USART_SendData(USART6, 0x79);

The response I read on terminal 0b1111 1001(Dec: 159)(Hx: F9)

Thanks in advanced.

Yigit

This discussion is locked. Please start a new topic to ask your question.
19 REPLIES 19
Posted on October 18, 2017 at 12:26

I guess some bits is missing, it could be stopbit but why is the stopbit missing?

Dunno, perhaps the Serial/USB converter does not support all settings.

I would check a 0xAA and 0x55 pattern, with a scope.

And I'm still not sure if the settings for your PC terminal application are correct.

TX(F407)                                                     RX(TeraTerm)

0b

01

11 1001 ------------------------------------> 0b

11

11 1001

0b

01

00 0111

 ------------------------------------>

 0b

10

00 0111

0b

01

01 0100 

 ----------------------------------->

 0b

10

01 0100

Rather looks like a problem with the first bits.

waclawek.jan
Super User
Posted on October 18, 2017 at 14:27

Read out and post the RCC and UART registers content.

JW

Posted on October 18, 2017 at 13:13

Unsurprisingly, this settings seem to match those of the F407.

But what stands out, at least for me :

GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP;

I initialized this pins always with GPIO_PuPd_NOPULL, which worked for me.

Posted on October 18, 2017 at 13:45

I don't see an immediate problem with the clock settings.

And according to my experience, a core clock mismatch looks different.

You receive just garbage, not at all resembling the sent values.

What is suspicious - PC7 is connected to the MCLK input of the audio codec (CS43L22).

There seems no alternative route for UART6 RX - have you tried another UART ?

Posted on October 18, 2017 at 14:04

it is happen beacuse of 'HSE_VALUE' symbolic constant it was not equal to actual crystal value, how I forgot the fix it,

Can you tell us the difference between the specified and the actual value ?

The 'usual' case was 25 MHz instead of 8 MHz when using the SPL (default quartz on ST eval boards vs. ST disco boards).

And that looked >>very<< different.

Your freqencies must have been quite close.

Posted on October 18, 2017 at 14:17

Hello!

Inside stm32f4xx.h the default HSE value is 25000000

Discovery's crystal is 8000000 Hz

Tamas Novak
Associate III
Posted on October 19, 2017 at 10:39

Hi, the problem is with your RS232 analyzer: the oscilloscope image you attached shows a perfect 0x79. 

- serial comm starts with a start bit (the first low level part before point 'a')

- then 8 bit data starting with the least sigificant bit (0x79= 0111 1001,but in order it is 10011110)

- parity bit (if enabled)

- stop bit (H level)

- idle (H level) if no immediate next byte

So the sequence you need to see (in real order) is:

0(start bit) - 10011110 (data, LSB first) - 0(parity bit) - 1(stopbit)

(you can't really see stop bit, as it is the same level as the idle following)

Check your recording, everything fine.

Posted on October 19, 2017 at 10:52

I mean sorry I didn't noticed that parity is disabled in your initialization code. Oscillogram shows the good 0x79 but with parity. 

One more thing: a-b time is 109.9usec.  Exact bit time is 104.2usec, so this 5.5% difference may corrupt communication if the receiver side also has a difference in the opposite direction.

I'd measure a longer period for higher accuracy: from the first H->L edge (start of startbit) to the last L->H (start of stopbit) it should be 9 (witohut parity) or 10 (paritiy enabled)  bit times, so 937.5 or 1041.7 usec.

Posted on October 19, 2017 at 10:52

That would be right, but at 9216Baud, not at 9600.

The problem is in timing, i.e. in clocking of the USART, and possibly the whole mcu.

JW

Posted on October 19, 2017 at 11:13

Sorry Jan, I didn't check all the posts.

Anyway the whole case doesn't fit: the oscillogram seems a 9600bps comm with parity and a slighty differing clock.  Its bit time is surely not shrinked or widened  by 8/25x or 25/8x ratio ...

Okay, I see case is closed, gotta leave it:)))