cancel
Showing results for 
Search instead for 
Did you mean: 

Error in the RM0090 Rev21

DenMir
Associate

Hi, I don't know where to post this message.

There's an error in the RM0090 Rev21 reference manual, page 121: "bit 15 of the PWR_CR register" should be "bit 14 of the PWR_CR register".

And most importantly, the debugger doesn't have bit 14 (VOS) of the PWR_CR register. I'm using an STM32F407ZET. I downloaded the archive https://www.st.com/resource/en/svd/stm32f4-svd.zip, and this bit is indeed missing from the STM32F407.svd file!

111.png

Please email whoever needs this information, and have them fix it.

1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hello @DenMir and welcome to the community;

 

Thank you for bringing these issues to our attention.

I reported these typos internally for checking and fixing.

Internal ticket number:

For reference manual issue: CDM0061028 (This is an internal tracking number and is not accessible or usable by customers).  

For SVD issue: CDM0061029 (This is an internal tracking number and is not accessible or usable by customers).  

 

Thank you for your contribution in STCommunity.

 

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
KDJEM.1
ST Employee

Hello @DenMir and welcome to the community;

 

Thank you for bringing these issues to our attention.

I reported these typos internally for checking and fixing.

Internal ticket number:

For reference manual issue: CDM0061028 (This is an internal tracking number and is not accessible or usable by customers).  

For SVD issue: CDM0061029 (This is an internal tracking number and is not accessible or usable by customers).  

 

Thank you for your contribution in STCommunity.

 

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.