2019-06-19 5:05 AM
Hello Everyone,
I have dealing with STM32F407 I2C peripheral in order to implement Non-blocking communication.
I have made many trials but I2C1 event and error interrupts never occur. I checked the SB bits during the debug mode it becomes 1,the other register seems okay but interrupt is never created. Also I have made different trials, changed interrupt priorities, enabled ev and er interrupts before enabling the periheral, after enabling periheral and after start condition is generated.
I have made other trials with cubemx and hal library for my board. After SB bit is set interrupt occured. However I couldn’t see the start bit from logic analyzer.
What am I missing here ?
I am using IAR 8.32, Here is my code ;
I2C.c
void I2C1_SystemInit(void ){
I2C1->CR1 &= ~I2C_CR1_PE; // I2C peripheral disable
// I2C1 Initialization PB8 (SCL) ve PB9 (SDA)
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOBEN; // Enable clock for GPIOB
GPIOB->AFR[1] |= (4); // PB8 AF4 for I2C1
GPIOB->AFR[1] |= (4 << 4); // PB9 AF4 for I2C1
GPIOB->MODER &= ~(3 << 16); // Clear bits 12 & 13 (PB8)
GPIOB->MODER |= GPIO_MODER_MODER8_1; // Set GPIOB8 to alternate function
GPIOB->MODER &= ~(3 << 18); // Clear bits 14 & 15 (PB9)
GPIOB->MODER |= GPIO_MODER_MODER9_1; // Set GPIOB9 to alternate function
GPIOB->OTYPER |= GPIO_OTYPER_OT_8; // Open Drain
GPIOB->OTYPER |= GPIO_OTYPER_OT_9; // Open Drain
GPIOB->PUPDR |= GPIO_PUPDR_PUPDR8_0; // Pull-Up
GPIOB->PUPDR |= GPIO_PUPDR_PUPDR9_0; // Pull-Up
GPIOB->OSPEEDR |= (3<<16);
GPIOB->OSPEEDR |= (3<<18);
RCC->APB1ENR |= RCC_APB1ENR_I2C1EN; // Enable clock for I2C1
I2C1->CR2 |= 0x14;
I2C1->CCR |= 208;
I2C1->TRISE |= 0x5; // 100 kHz
// I2C1->CR1 |= I2C_CR1_NOSTRETCH;
// I2C1->CR1 |= I2C_CR1_ACK; // Acknowledge enable
// I2C1->CR1 &= ~I2C_CR1_POS; // Disable Pos
// I2C1->CR2 |= I2C_CR2_ITEVTEN; //<Event Interrupt Enable
// I2C1->CR2 |= I2C_CR2_ITBUFEN; //<Buffer Interrupt Enable
// I2C1->CR2 |= I2C_CR2_ITERREN;
I2C1->CR1 |= I2C_CR1_PE;
}
void I2C1_EV_IRQHandler(void){
flag=1; uint32_t sr2itflags = (I2C1->SR2);
uint32_t sr1itflags = (I2C1->SR1);
uint32_t itsources = (I2C1->CR2); }
void I2C1_ER_IRQHandler(void){ flag=2; uint32_t sr2itflags = (I2C1->SR2);
uint32_t sr1itflags = (I2C1->SR1);
uint32_t itsources = (I2C1->CR2); }
Main.c
void Init_Priorities(void){
SCB->AIRCR = ((uint32_t)0x05FA0000) | NVIC_PriorityGroup_4; // NVIC_SetPriorityGrouping(4)
NVIC_SetPriority(TIM1_UP_TIM10_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
NVIC_SetPriority(ADC_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),1, 0));
NVIC_SetPriority(TIM1_BRK_TIM9_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),2, 0));
NVIC_SetPriority(TIM1_TRG_COM_TIM11_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),3, 0));
NVIC_SetPriority(TIM8_BRK_TIM12_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),4, 0));
NVIC_SetPriority(TIM8_TRG_COM_TIM14_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),5, 0));
NVIC_SetPriority(I2C1_EV_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),6, 0));
NVIC_SetPriority(I2C1_ER_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),7, 0));
NVIC_SetPriority(I2C2_EV_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),8, 0));
NVIC_SetPriority(I2C2_ER_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),9, 0));
}
void TIM8_TRG_COM_TIM14_IRQHandler(void) { RD_EEP1(); TIM14->SR &= ~(TIM_SR_UIF); }
void RD_EEP1(void){
if((I2C1->CR1 & I2C_CR1_PE) != I2C_CR1_PE){
I2C1->CR1 |= I2C_CR1_PE; } // I2C peripheral enable
I2C1->CR1 &= ~I2C_CR1_POS;
I2C1->CR1 |= I2C_CR1_START; asm("nop"); asm("nop"); asm("nop");
I2C1->CR2 |= I2C_CR2_ITEVTEN; //<Event Interrupt Enable
I2C1->CR2 |= I2C_CR2_ITBUFEN; //<Buffer Interrupt Enable
I2C1->CR2 |= I2C_CR2_ITERREN;
GREEN_LED_ON;
}
int main()
{ for(uint16_t i=0;i<10000;i++); // wait for a while K
Fan_Control(); // Fan pins initilization
init_inj_adc_interrupt(); // ADC Injected Channel
I2C1_SystemInit();
DAC1_Init();
TIM9_Init(); // 1mS Timer Interrupt Init
TIM11_Init(); // 10mS Timer Interrupt Init
TIM12_Init(); // 100mS Timer Interrupt Init
TIM14_Init(); // 1000mS Timer Interrupt Init
Init_Priorities();
while(1){
} }
Solved! Go to Solution.
2019-06-20 12:58 AM
Hello again, I found the problem guys,
change the code like this ;
void I2C1_SystemInit(void ){
// I2C1 Initialization PB8 (SCL) ve PB9 (SDA)
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOBEN; // Enable clock for GPIOB
GPIOB->AFR[1] |= (4); // PB8 AF4 for I2C1
GPIOB->AFR[1] |= (4 << 4); // PB9 AF4 for I2C1
GPIOB->MODER &= ~(3 << 16); // Clear bits 12 & 13 (PB8)
GPIOB->MODER |= GPIO_MODER_MODER8_1; // Set GPIOB8 to alternate
GPIOB->MODER &= ~(3 << 18); // Clear bits 14 & 15 (PB9)
GPIOB->MODER |= GPIO_MODER_MODER9_1; // Set GPIOB9 to alternate
GPIOB->OTYPER |= GPIO_OTYPER_OT_8;
GPIOB->OTYPER |= GPIO_OTYPER_OT_9;
GPIOB->PUPDR |= GPIO_PUPDR_PUPDR8_0; // pull-up,
GPIOB->PUPDR |= GPIO_PUPDR_PUPDR9_0; // pull-up,
GPIOB->OSPEEDR |= (3<<16);
GPIOB->OSPEEDR |= (3<<18);
RCC->APB1ENR |= RCC_APB1ENR_I2C1EN; // Enable clock for I2C1
while(!(RCC->APB1ENR & RCC_APB1ENR_I2C1EN) ){}
for(uint16_t i=0;i<1000;i++);
NVIC_SetPriority(I2C1_EV_IRQn, 6);
NVIC_EnableIRQ(I2C1_EV_IRQn);
NVIC_SetPriority(I2C1_ER_IRQn, 7);
NVIC_EnableIRQ(I2C1_ER_IRQn);
I2C1->CR1 &= ~I2C_CR1_PE; // I2C peripheral disable
I2C1->CR2 |= 0x2A; //0x14;
I2C1->CCR |= 0X0D2; //208;
I2C1->TRISE |= 0x2B; //0x5;
I2C1->CR1 |= I2C_CR1_PE;
for(uint16_t i=0;i<1000;i++);
}
2019-06-20 12:58 AM
Hello again, I found the problem guys,
change the code like this ;
void I2C1_SystemInit(void ){
// I2C1 Initialization PB8 (SCL) ve PB9 (SDA)
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOBEN; // Enable clock for GPIOB
GPIOB->AFR[1] |= (4); // PB8 AF4 for I2C1
GPIOB->AFR[1] |= (4 << 4); // PB9 AF4 for I2C1
GPIOB->MODER &= ~(3 << 16); // Clear bits 12 & 13 (PB8)
GPIOB->MODER |= GPIO_MODER_MODER8_1; // Set GPIOB8 to alternate
GPIOB->MODER &= ~(3 << 18); // Clear bits 14 & 15 (PB9)
GPIOB->MODER |= GPIO_MODER_MODER9_1; // Set GPIOB9 to alternate
GPIOB->OTYPER |= GPIO_OTYPER_OT_8;
GPIOB->OTYPER |= GPIO_OTYPER_OT_9;
GPIOB->PUPDR |= GPIO_PUPDR_PUPDR8_0; // pull-up,
GPIOB->PUPDR |= GPIO_PUPDR_PUPDR9_0; // pull-up,
GPIOB->OSPEEDR |= (3<<16);
GPIOB->OSPEEDR |= (3<<18);
RCC->APB1ENR |= RCC_APB1ENR_I2C1EN; // Enable clock for I2C1
while(!(RCC->APB1ENR & RCC_APB1ENR_I2C1EN) ){}
for(uint16_t i=0;i<1000;i++);
NVIC_SetPriority(I2C1_EV_IRQn, 6);
NVIC_EnableIRQ(I2C1_EV_IRQn);
NVIC_SetPriority(I2C1_ER_IRQn, 7);
NVIC_EnableIRQ(I2C1_ER_IRQn);
I2C1->CR1 &= ~I2C_CR1_PE; // I2C peripheral disable
I2C1->CR2 |= 0x2A; //0x14;
I2C1->CCR |= 0X0D2; //208;
I2C1->TRISE |= 0x2B; //0x5;
I2C1->CR1 |= I2C_CR1_PE;
for(uint16_t i=0;i<1000;i++);
}