STM32F405RG 시리즈 문�?�
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-06-28 5:32 PM
안녕하세요.
기존�? 사용중�?� 시스템 (PIC 계열) �?서 MCU 만 �?체를 하여 사용�?� 하려고 합니다.
기본 Digital I/O 신호가 5V �?��?�요.
STM32F405RG �?� Datasheet 를 보면서 �?금�?�?� 있어 문�?�를 드립니다.
I/O structure 가 FT �?� 경우, 기존 사용하면 신호를 그대로 연결�?� 해�?� 무방한지요?
아니면 Level shift 회로를 추가하는게 좋�?�지요?
- Labels:
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-06-30 8:27 AM
Hi @CJeon.1 ,
First of all, welcome to ST Community!
As the common used language in this community is English, I tried to translate your question and I got this result:
*****************************************************
STM32F405RG series inquiry
Good morning.
I want to use it by replacing only the MCU in the existing system (PIC series).
The basic digital I/O signal is 5V.
I have a question while looking at the datasheet of STM32F405RG, so please inquire
If the I/O structure is FT, is it okay to connect the signal as it is if it is used in the past?
Or is it better to add a level shift circuit?
*****************************************************
I am not sure to fully understand it based on this translation. So please explain it more.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.