2023-10-18 08:22 AM
Hello,
We are looking at using a STM32F405 in our power design LLC/PFC where we would need 4 complementary signals. 2 for the LLC and 2 for the PFC.
Looking at the reference manual I see the following:
17.3.11 Complementary outputs and dead-time insertion
The advanced-control timers (TIM1 and TIM8) can output two complementary signals and
manage the switching-off and the switching-on instants of the outputs.
So, it looks like for this part there is only the two complementary signals on TIM1 and TIM8?
Thanks for any insight.
Brent
Solved! Go to Solution.
2023-10-18 09:09 AM
TIM1 and TIM8 each have 3 complimentary channels. CH4N isn't available on either.
They are on independent pins, so a total of 6 channels are available.
2023-10-18 09:09 AM
TIM1 and TIM8 each have 3 complimentary channels. CH4N isn't available on either.
They are on independent pins, so a total of 6 channels are available.