cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F401RBT6 HSE Clock Issue with TCXO

Alaeddine_Chamsi
Associate II

I’m designing a board with the STM32F401RBT6 and have decided to use a 48 MHz TCXO for the HSE clock.
I’ve written a simple "Hello World" program that communicates through USART.
the TCXO i used : TG2016SMN 48.0000M-MCGNNM3 
Observations: When using the HSI (internal oscillator), the program works fine. When switching to the HSE (with the TCXO), the program does not work. I measured the TCXO OUTPUT SIGNAL using an oscilloscope. The waveform is shown in the attached image.image00001.jpeg

 

Capture d'écran 2025-01-16 192953.png

 value of R8 and R9 = 0 , C13 = 10 pF , C16 = 1000pF 
What could be causing the program to fail with the HSE clock? Are there any specific considerations or configurations required to use a TCXO with the HSE input on this MCU?

 

7 REPLIES 7
STOne-32
ST Employee

Dear @Alaeddine_Chamsi ,

 

Welcome in STCommunity and thank you for sharing your use case .  

1) Can You try to remove R9 so to leave PH1 Open .

2) by software, did you switched the HSE ON and in bypass mode ? Out of reset as you have seen HSI is always ON . 

3) How do you know the program is not working ?  Can you share where the code is stuck ? Using the debugger . You can put a LED blinking infinite loop and let us know .

Hope it helps you . 
STOne-32

 

Dear @STOne-32 ,
Thank you for your warm welcome and for taking the time to guide me through my issue.

I appreciate your suggestions and have reviewed them in detail. Below are my responses and additional details:
1) I tried removing R9 to leave PH1 open as you suggested and nothing changed.
2) Regarding the software configuration, I have enabled HSE and set it to bypass mode. Please find my SystemClock_Config code attached below for your review.

 

void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; // Configure the main internal regulator output voltage __HAL_RCC_PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1); // Initializes the TCXO oscillator RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 8; RCC_OscInitStruct.PLL.PLLN = 336; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 7; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { // Initialization Error Error_Handler(); } // Initializes the CPU, AHB and APB buses clocks RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK) { // Initialization Error Error_Handler(); } } void Error_Handler(void) { // User can add his own implementation to report the HAL error return state while(1) { } }
View more

 


Additionally, I have attached my complete code and the schematic of my setup for your reference.
Please let me know if there’s anything else I can check or modify.
473642189_1648740859394820_8816937521150131920_n.png

 

#include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ TIM_HandleTypeDef htim1; TIM_HandleTypeDef htim3; UART_HandleTypeDef huart1; UART_HandleTypeDef huart2; UART_HandleTypeDef huart6; /* USER CODE BEGIN PV */ // Message to send over UART /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ TIM_HandleTypeDef htim3; UART_HandleTypeDef huart1; UART_HandleTypeDef huart2; UART_HandleTypeDef huart6; /* USER CODE BEGIN PV */ /* USER CODE BEGIN PV */ uint32_t ICValue = 0; uint32_t Frequency = 0; float Duty = 0; uint32_t RisingEdges = 0; /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_USART1_UART_Init(void); static void MX_USART2_UART_Init(void); static void MX_USART6_UART_Init(void); static void MX_TIM3_Init(void); static void MX_TIM1_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim) { if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) { // Increment rising edge count RisingEdges++; // Read the ICValue ICValue = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_1); } if (ICValue != 0) { // Calculate the duty cycle and frequency Duty = (HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_2) * 100) / ICValue; Frequency = 84000000 / ICValue; } } /** * @brief The application entry point. * @retval int */ void TransmitHelloWorld() { char buffer[100]; uint32_t DutyInt = (uint32_t)(Duty * 100); snprintf(buffer, sizeof(buffer), "Hello World! Frequency: %lu Hz, Duty: %lu.%02lu%%\r\n", Frequency, DutyInt / 100, DutyInt % 100); // Transmit via UART1 HAL_UART_Transmit(&huart1, (uint8_t *)buffer, strlen(buffer), HAL_MAX_DELAY); // Transmit via UART2 HAL_UART_Transmit(&huart2, (uint8_t *)buffer, strlen(buffer), HAL_MAX_DELAY); // Transmit via UART6 HAL_UART_Transmit(&huart6, (uint8_t *)buffer, strlen(buffer), HAL_MAX_DELAY); } int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_USART1_UART_Init(); MX_USART2_UART_Init(); MX_USART6_UART_Init(); MX_TIM3_Init(); /* USER CODE BEGIN 2 */ HAL_TIM_IC_Start_IT(&htim3, TIM_CHANNEL_1); // Start input capture interrupt on channel 1 HAL_TIM_IC_Start(&htim3, TIM_CHANNEL_2); // Start input capture on channel 2 /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { TransmitHelloWorld(); // Send "Hello World" message with values HAL_Delay(1000); // 1-second delay } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; // Configure the main internal regulator output voltage __HAL_RCC_PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1); // Initializes the TCXO oscillator RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 8; RCC_OscInitStruct.PLL.PLLN = 336; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 7; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { // Initialization Error Error_Handler(); } // Initializes the CPU, AHB and APB buses clocks RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK) { // Initialization Error Error_Handler(); } } void Error_Handler(void) { // User can add his own implementation to report the HAL error return state while(1) { } } /** * @brief TIM1 Initialization Function * @param None * @retval None */ static void MX_TIM1_Init(void) { /* USER CODE BEGIN TIM1_Init 0 */ /* USER CODE END TIM1_Init 0 */ TIM_ClockConfigTypeDef sClockSourceConfig = {0}; TIM_MasterConfigTypeDef sMasterConfig = {0}; /* USER CODE BEGIN TIM1_Init 1 */ /* USER CODE END TIM1_Init 1 */ htim1.Instance = TIM1; htim1.Init.Prescaler = 0; htim1.Init.CounterMode = TIM_COUNTERMODE_UP; htim1.Init.Period = 65535; htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim1.Init.RepetitionCounter = 0; htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; if (HAL_TIM_Base_Init(&htim1) != HAL_OK) { Error_Handler(); } sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM1_Init 2 */ /* USER CODE END TIM1_Init 2 */ } /** * @brief TIM3 Initialization Function * @param None * @retval None */ static void MX_TIM3_Init(void) { /* USER CODE BEGIN TIM3_Init 0 */ /* USER CODE END TIM3_Init 0 */ TIM_ClockConfigTypeDef sClockSourceConfig = {0}; TIM_SlaveConfigTypeDef sSlaveConfig = {0}; TIM_IC_InitTypeDef sConfigIC = {0}; TIM_MasterConfigTypeDef sMasterConfig = {0}; /* USER CODE BEGIN TIM3_Init 1 */ /* USER CODE END TIM3_Init 1 */ htim3.Instance = TIM3; htim3.Init.Prescaler = 0; htim3.Init.CounterMode = TIM_COUNTERMODE_UP; htim3.Init.Period = 65535; htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; if (HAL_TIM_Base_Init(&htim3) != HAL_OK) { Error_Handler(); } sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK) { Error_Handler(); } if (HAL_TIM_IC_Init(&htim3) != HAL_OK) { Error_Handler(); } sSlaveConfig.SlaveMode = TIM_SLAVEMODE_RESET; sSlaveConfig.InputTrigger = TIM_TS_TI1FP1; sSlaveConfig.TriggerPolarity = TIM_INPUTCHANNELPOLARITY_RISING; sSlaveConfig.TriggerPrescaler = TIM_ICPSC_DIV1; sSlaveConfig.TriggerFilter = 0; if (HAL_TIM_SlaveConfigSynchro(&htim3, &sSlaveConfig) != HAL_OK) { Error_Handler(); } sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING; sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI; sConfigIC.ICPrescaler = TIM_ICPSC_DIV1; sConfigIC.ICFilter = 0; if (HAL_TIM_IC_ConfigChannel(&htim3, &sConfigIC, TIM_CHANNEL_1) != HAL_OK) { Error_Handler(); } sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_FALLING; sConfigIC.ICSelection = TIM_ICSELECTION_INDIRECTTI; if (HAL_TIM_IC_ConfigChannel(&htim3, &sConfigIC, TIM_CHANNEL_2) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM3_Init 2 */ /* USER CODE END TIM3_Init 2 */ } /** * @brief USART1 Initialization Function * @param None * @retval None */ static void MX_USART1_UART_Init(void) { /* USER CODE BEGIN USART1_Init 0 */ /* USER CODE END USART1_Init 0 */ /* USER CODE BEGIN USART1_Init 1 */ /* USER CODE END USART1_Init 1 */ huart1.Instance = USART1; huart1.Init.BaudRate = 115200; huart1.Init.WordLength = UART_WORDLENGTH_8B; huart1.Init.StopBits = UART_STOPBITS_1; huart1.Init.Parity = UART_PARITY_NONE; huart1.Init.Mode = UART_MODE_TX_RX; huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart1.Init.OverSampling = UART_OVERSAMPLING_16; if (HAL_UART_Init(&huart1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART1_Init 2 */ /* USER CODE END USART1_Init 2 */ } /** * @brief USART2 Initialization Function * @param None * @retval None */ static void MX_USART2_UART_Init(void) { /* USER CODE BEGIN USART2_Init 0 */ /* USER CODE END USART2_Init 0 */ /* USER CODE BEGIN USART2_Init 1 */ /* USER CODE END USART2_Init 1 */ huart2.Instance = USART2; huart2.Init.BaudRate = 115200; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; if (HAL_UART_Init(&huart2) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART2_Init 2 */ /* USER CODE END USART2_Init 2 */ } /** * @brief USART6 Initialization Function * @param None * @retval None */ static void MX_USART6_UART_Init(void) { /* USER CODE BEGIN USART6_Init 0 */ /* USER CODE END USART6_Init 0 */ /* USER CODE BEGIN USART6_Init 1 */ /* USER CODE END USART6_Init 1 */ huart6.Instance = USART6; huart6.Init.BaudRate = 115200; huart6.Init.WordLength = UART_WORDLENGTH_8B; huart6.Init.StopBits = UART_STOPBITS_1; huart6.Init.Parity = UART_PARITY_NONE; huart6.Init.Mode = UART_MODE_TX_RX; huart6.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart6.Init.OverSampling = UART_OVERSAMPLING_16; if (HAL_UART_Init(&huart6) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART6_Init 2 */ /* USER CODE END USART6_Init 2 */ } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ }
View more

 

Thank you again for your valuable assistance. Your expertise is greatly appreciated!

Best regards,
Alaeddine Chamsi


 

With MCU capacitor on OUT is fail. Replace C16 with 0-33R

// Initializes the TCXO oscillator RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 8; RCC_OscInitStruct.PLL.PLLN = 336; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 7;

plus this never can work with 48M

Danish1
Lead III

The timebase on your oscilloscope is set to 20ms / division. That will not show 48MHz.

What you are showing is the waveform aliased-down by the 25000 samples per second sampling-rate that your oscilloscope uses when running at such a slow timebase.

You need to increase the oscilloscope timebase to something like 0.1 microseconds per division to have a hope of seeing the waveform (or better 0.02 microseconds per division if your oscilloscope will go that fast).

And the other thing is that the voltage you present to PH0 needs to swing from below 0.3 x Vdd to above 0.7 x Vdd, so that means that at a typical 3.3V supply it needs to swing from below 0.99V to above 2.31V.

The schematic shows you AC-coupling the output of the oscillator and biasing it around 0.0V (C16 and R7). And then C13 attenuates the signal. This will not work.

Remove all three of those components. Instead of C16 fit a resistor (you can use R7 if that's convenient).

Thank you for your detailed explanation! I tested this on two boards:

  1. On the first board, I removed C16, C13, and R7 as you suggested. The signal on PH0 now swings from -370 mV to 1.20 V (shown in Picture 1).
  2. On the second board, I only removed C16 and kept R7 and C13, since the TCXO datasheet recommends this RC load. In this case, the signal swings from -290 mV to 1.10 V (shown in Picture 2).

Would you have any suggestions on how I could improve this further? I really appreciate your guidance! :smiling_face_with_smiling_eyes:


removed C16, C13, and R7removed C16, C13, and R7only removed C16 and kept R7 and C13only removed C16 and kept R7 and C13

Primary switch scope to 1:10 

MM1_0-1739621720442.png

1:1 is limited around to 10MHz

And still your connection to MCU is fail. For active TCXO R9 / PH1 must be unconnected

thank you for your response, R9 is already removed in both boards and i I have enabled HSE and set it to bypass mode.